![]() |
Vision Apps User Guide
|
DOF flow vectors to track parameters. More...
#include <tivx_park_assist_kernels.h>
DOF flow vectors to track parameters.
| vx_uint32 tivx_dof_to_tracks_params_t::dofConfidThresh |
max DOF confidence to be considered, valid range 0 (low confidence) to 15 (high confidence)
| tivx_dof_to_tracks_roi_type_e tivx_dof_to_tracks_params_t::roiType |
the ROI type used
| vx_float32 tivx_dof_to_tracks_params_t::roiPrm1 |
ROI param 1 (see tivx_dof_to_tracks_roi_type)
| vx_float32 tivx_dof_to_tracks_params_t::roiPrm2 |
ROI param 2 (see tivx_dof_to_tracks_roi_type)
| uint32_t tivx_dof_to_tracks_params_t::subsampleFactor |
sub sample factor for picking flow vectors from DOF
| vx_float32 tivx_dof_to_tracks_params_t::focalLength |
focal length of camera lens [pixels]
| vx_float32 tivx_dof_to_tracks_params_t::principalPointX |
x-coordinate of camera's principal point [pixels]
| vx_float32 tivx_dof_to_tracks_params_t::principalPointY |
y-coordinate of camera's principal point [pixels]
| vx_float32 tivx_dof_to_tracks_params_t::d2uTableStep |
Distorted to Undistorted Table step (needs to correspond to node's lut input