![]() |
Vision Apps User Guide
|
Heap initialization parameters. More...
#include <app_mem.h>
Data Fields | |
| void * | base |
| char | name [APP_MEM_HEAP_NAME_MAX] |
| uint32_t | size |
| uint32_t | flags |
Heap initialization parameters.
| void* app_mem_heap_prm_t::base |
heap memory base address
| char app_mem_heap_prm_t::name[APP_MEM_HEAP_NAME_MAX] |
heap name
| uint32_t app_mem_heap_prm_t::size |
heap size in bytes
| uint32_t app_mem_heap_prm_t::flags |
flags, see APP_MEM_HEAP_FLAGS