![]() |
TIOVX User Guide
|
Remap object descriptor as placed in shared memory. More...
#include <tivx_obj_desc.h>
Data Fields | |
| tivx_obj_desc_t | base |
| base object descriptor | |
| tivx_shared_mem_ptr_t | mem_ptr |
| buffer address | |
| volatile uint32_t | src_width |
| The source width. | |
| volatile uint32_t | src_height |
| The source height. | |
| volatile uint32_t | dst_width |
| The destination width. | |
| volatile uint32_t | dst_height |
| The destination height. | |
| volatile uint32_t | mem_size |
| size of buffer pointed to by mem_ptr | |
Remap object descriptor as placed in shared memory.
Definition at line 539 of file tivx_obj_desc.h.