PDK API Guide for AM65xx

Introduction

Functions

Uint32 CSL_CPGMAC_SL_isFullDuplexEnabled (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_enableFullDuplex (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_disableFullDuplex (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
Uint32 CSL_CPGMAC_SL_isLoopbackModeEnabled (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_enableLoopback (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_disableLoopback (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
Uint32 CSL_CPGMAC_SL_isRxFlowControlEnabled (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_enableRxFlowControl (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_disableRxFlowControl (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
Uint32 CSL_CPGMAC_SL_isTxFlowControlEnabled (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_enableTxFlowControl (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_disableTxFlowControl (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
Uint32 CSL_CPGMAC_SL_isGMIIEnabled (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_enableGMII (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_disableGMII (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
Uint32 CSL_CPGMAC_SL_isTxPaceEnabled (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_enableTxPace (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_disableTxPace (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
Uint32 CSL_CPGMAC_SL_isGigabitEnabled (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_enableGigabit (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_disableGigabit (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
Uint32 CSL_CPGMAC_SL_isTxShortGapEnabled (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_enableTxShortGap (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_disableTxShortGap (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
Uint32 CSL_CPGMAC_SL_isIdleModeEnabled (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_enableIdleMode (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_disableIdleMode (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
Uint32 CSL_CPGMAC_SL_isCastagnoliCRCEnabled (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_enableCastagnoliCRC (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_disableCastagnoliCRC (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
Uint32 CSL_CPGMAC_SL_isIFCTLAEnabled (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_enableIFCTLA (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_disableIFCTLA (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
Uint32 CSL_CPGMAC_SL_isIFCTLBEnabled (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_enableIFCTLB (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_disableIFCTLB (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
Uint32 CSL_CPGMAC_SL_isGigForceModeEnabled (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_enableGigForceMode (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_disableGigForceMode (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
Uint32 CSL_CPGMAC_SL_isExtControlEnabled (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_enableExtControl (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_disableExtControl (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
Uint32 CSL_CPGMAC_SL_isExtRxFlowEnabled (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_enableExtRxFlow (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_disableExtRxFlow (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
Uint32 CSL_CPGMAC_SL_isExtTxFlowEnabled (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_enableExtTxFlow (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_disableExtTxFlow (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
Uint32 CSL_CPGMAC_SL_isRxCEFEnabled (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_enableRxCEF (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_disableRxCEF (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
Uint32 CSL_CPGMAC_SL_isRxCSFEnabled (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_enableRxCSF (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_disableRxCSF (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
Uint32 CSL_CPGMAC_SL_isRxCMFEnabled (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_enableRxCMF (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_disableRxCMF (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
Uint32 CSL_CPGMAC_SL_getMacControlReg (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_setMacControlReg (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum, Uint32 macControlRegVal)
 
void CSL_CPGMAC_SL_getMacStatusReg (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum, CSL_CPGMAC_SL_MACSTATUS *pMacStatus)
 
void CSL_CPGMAC_SL_resetMac (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
Uint32 CSL_CPGMAC_SL_isMACResetDone (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
Uint32 CSL_CPGMAC_SL_getRxMaxLen (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
Uint32 CSL_CPGMAC_SL_setRxMaxLen (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum, Uint32 rxMaxLen)
 
Uint32 CSL_CPGMAC_SL_getTxGap (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
Uint32 CSL_CPGMAC_SL_setTxGap (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum, Uint32 txGap)
 
Uint32 CSL_CPGMAC_SL_getRxPauseTimerReg (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
Uint32 CSL_CPGMAC_SL_setRxPauseTimerReg (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum, Uint32 rxPauseTimer)
 
Uint32 CSL_CPGMAC_SL_getTxPauseTimerReg (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
Uint32 CSL_CPGMAC_SL_setTxPauseTimerReg (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum, Uint32 txPauseTimer)
 
void CSL_CPGMAC_SL_getEmulControlReg (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum, Uint32 *pEmulFreeBit, Uint32 *pEmulSoftBit)
 
void CSL_CPGMAC_SL_setEmulControlReg (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum, Uint32 emulFreeBit, Uint32 emulSoftBit)
 
void CSL_CPGMAC_SL_getMacRxPriMapReg (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum, Uint32 *pMacRxPriMap)
 
void CSL_CPGMAC_SL_setMacRxPriMapReg (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum, Uint32 *pMacRxPriMap)
 
void CSL_CPGMAC_SL_clearMacStatusTorf (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_clearMacStatusTorfPri (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_getInterVLANCfg (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum, Uint32 routeIndex, CSL_CPSW_INTERVLANCFG *pInterVLANCfg)
 
void CSL_CPGMAC_SL_setInterVLANCfg (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum, Uint32 routeIndex, CSL_CPSW_INTERVLANCFG *pInterVLANCfg)
 
void CSL_CPGMAC_SL_getFifoStatus (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum, CSL_CPGMAC_SL_FIFOSTATUS *pFifoStatus)
 
Uint32 CSL_CPGMAC_SL_isTxShortGapLimitEnabled (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_enableTxShortGapLimit (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 
void CSL_CPGMAC_SL_disableTxShortGapLimit (CSL_Xge_cpswRegs *hCpswRegs, Uint32 portNum)
 

Function Documentation

Uint32 CSL_CPGMAC_SL_isFullDuplexEnabled ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_isFullDuplexEnabled

Description
This function indicates if Full duplex mode is enabled in the MAC control register for the MAC port specified.

Arguments

       portNum                 MAC port number for which the API must retrieve the
                               settings.
*    

Return Value
TRUE Full duplex mode enabled
FALSE Half duplex mode enabled.

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_MAC_CONTROL_REG_FULLDUPLEX

Example

       Uint32 portNum;

       portNum =   1;
       if (CSL_CPGMAC_SL_isFullDuplexEnabled (portNum) == TRUE)
       {
           // full duplex mode enabled
       }
       else
       {
           // full duplex mode disabled
       }

void CSL_CPGMAC_SL_enableFullDuplex ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_enableFullDuplex

Description
This function configures the MAC control register to enable full duplex mode for the MAC port number specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_FULLDUPLEX=1

Example

*      Uint32      portNum =   1;

       CSL_CPGMAC_SL_enableFullDuplex (portNum);

void CSL_CPGMAC_SL_disableFullDuplex ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_disableFullDuplex

Description
This function configures the MAC control register to disable full duplex mode for the MAC port specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_FULLDUPLEX=0

Example

*      Uint32  portNum = 1;

       CSL_CPGMAC_SL_disableFullDuplex (portNum);

Uint32 CSL_CPGMAC_SL_isLoopbackModeEnabled ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_isLoopbackModeEnabled

Description
This function indicates if loopback mode is enabled in the MAC control register for the MAC port specified.

Arguments

       portNum                 MAC port number for which the API must
                               retrieve the settings.
*    

Return Value
TRUE Internal full duplex lopoback mode enabled
FALSE Loopback mode disabled.

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_MAC_CONTROL_REG_LOOPBACK

Example

*      Uint32  portNum = 1;

       if (CSL_CPGMAC_SL_isLoopbackModeEnabled (portNum) == TRUE)
       {
           // loopback mode enabled
       }
       else
       {
           // loopback mode disabled
       }

void CSL_CPGMAC_SL_enableLoopback ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_enableLoopback

Description
This function configures the MAC control register to enable lopback mode for the MAC port specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_LOOPBACK=1

Example

       Uint32  portNum = 1;

       CSL_CPGMAC_SL_enableLoopback (portNum);

void CSL_CPGMAC_SL_disableLoopback ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_disableLoopback

Description
This function configures the MAC control register to disable loopback mode for the MAC port specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_LOOPBACK=0

Example

       Uint32  portNum =   1;

       CSL_CPGMAC_SL_disableLoopback (portNum);

Uint32 CSL_CPGMAC_SL_isRxFlowControlEnabled ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_isRxFlowControlEnabled

Description
This function indicates if receive flow control is enabled in the MAC control register for the MAC port specified.

Arguments

       portNum                 MAC port number for which the API must
                               retrieve the settings.
*    

Return Value
TRUE Receive flow control enabled
FALSE Receive flow control disabled

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_MAC_CONTROL_REG_RX_FLOW_EN

Example

*      Uint32  portNum = 1;

       if (CSL_CPGMAC_SL_isRxFlowControlEnabled (portNum) == TRUE)
       {
           // rx flow control enabled
       }
       else
       {
           // rx flow control disabled
       }

void CSL_CPGMAC_SL_enableRxFlowControl ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_enableRxFlowControl

Description
This function configures the MAC control register to enable receive flow control for the MAC port specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_RX_FLOW_EN=1

Example

       Uint32  portNum =   1;

       CSL_CPGMAC_SL_enableRxFlowControl (portNum);

void CSL_CPGMAC_SL_disableRxFlowControl ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_disableRxFlowControl

Description
This function configures the MAC control register to disable Receive flow control mode for the MAC port specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_RX_FLOW_EN=0

Example

       Uint32  portNum =   1;

       CSL_CPGMAC_SL_disableRxFlowControl (portNum);

Uint32 CSL_CPGMAC_SL_isTxFlowControlEnabled ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_isTxFlowControlEnabled

Description
This function indicates if transmit flow control is enabled in the MAC control register for the MAC port specified.

Arguments

       portNum                 MAC port number for which the API must
                               retrieve the settings.
*    

Return Value
TRUE Transmit flow control enabled
FALSE Transmit flow control disabled

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_MAC_CONTROL_REG_TX_FLOW_EN

Example

*      Uint32  portNum =   1;

       if (CSL_CPGMAC_SL_isTxFlowControlEnabled (portNum) == TRUE)
       {
           // tx flow control enabled
       }
       else
       {
           // tx flow control disabled
       }

void CSL_CPGMAC_SL_enableTxFlowControl ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_enableTxFlowControl

Description
This function configures the MAC control register to enable transmit flow control for the MAC port specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_TX_FLOW_EN=1

Example

       Uint32  portNum =   1;

       CSL_CPGMAC_SL_enableTxFlowControl (portNum);

void CSL_CPGMAC_SL_disableTxFlowControl ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_disableTxFlowControl

Description
This function configures the MAC control register to disable Transmit flow control for the MAC port specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_TX_FLOW_EN=0

Example

       Uint32  portNum =   1;

       CSL_CPGMAC_SL_disableTxFlowControl (portNum);

Uint32 CSL_CPGMAC_SL_isGMIIEnabled ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_isGMIIEnabled

Description
This function indicates if GMII is enabled in the MAC control register for the MAC port specified.

Arguments

       portNum                 MAC port number for which the API must
                               retrieve the settings.
*    

Return Value
TRUE GMII enabled
FALSE GMII disabled

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_MAC_CONTROL_REG_GMII_EN

Example

*      Uint32  portNum =   1;

       if (CSL_CPGMAC_SL_isGMIIEnabled (portNum) == TRUE)
       {
           // gmii enabled
       }
       else
       {
           // gmii disabled
       }

void CSL_CPGMAC_SL_enableGMII ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_enableGMII

Description
This function configures the MAC control register to enable GMII for the MAC port specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_GMII_EN=1

Example

       Uint32  portNum =   1;

       CSL_CPGMAC_SL_enableGMII (portNum);

void CSL_CPGMAC_SL_disableGMII ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_disableGMII

Description
This function configures the MAC control register to disable GMII for the MAC port specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_GMII_EN=0

Example

       Uint32  portNum =   1;

       CSL_CPGMAC_SL_disableGMII (portNum);

Uint32 CSL_CPGMAC_SL_isTxPaceEnabled ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_isTxPaceEnabled

Description
This function indicates if transmit pacing is enabled in the MAC control register for the MAC port specified.

Arguments

       portNum                 MAC port number for which the API must
                               retrieve the settings.
*    

Return Value
TRUE Transmit pacing enabled
FALSE Transmit pacing disabled

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_MAC_CONTROL_REG_TX_PACE

Example

*      Uint32  portNum =   1;

       if (CSL_CPGMAC_SL_isTxPaceEnabled (portNum) == TRUE)
       {
           // tx pacing enabled
       }
       else
       {
           // tx pacing disabled
       }

void CSL_CPGMAC_SL_enableTxPace ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_enableTxPace

Description
This function configures the MAC control register to enable transmit pacing for the MAC port specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_TX_PACE=1

Example

       Uint32  portNum = 1;

       CSL_CPGMAC_SL_enableTxPace (portNum);

void CSL_CPGMAC_SL_disableTxPace ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_disableTxPace

Description
This function configures the MAC control register to disable transmit pacing for the MAC port specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_TX_PACE=0

Example

       Uint32  portNum = 1;

       CSL_CPGMAC_SL_disableTxPace (portNum);

Uint32 CSL_CPGMAC_SL_isGigabitEnabled ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_isGigabitEnabled

Description
This function indicates if Gigabit mode is enabled in the MAC control register for the MAC port specified.

Arguments

       portNum                 MAC port number for which the API must
                               retrieve the settings.
*    

Return Value
TRUE Gigabit mode enabled
FALSE Gigabit disabled. 10/100 mode enabled.

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_MAC_CONTROL_REG_GIG

Example

*      Uint32  portNum = 1;

       if (CSL_CPGMAC_SL_isGigabitEnabled (portNum) == TRUE)
       {
           // gig enabled
       }
       else
       {
           // gig disabled
       }

void CSL_CPGMAC_SL_enableGigabit ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_enableGigabit

Description
This function configures the MAC control register to enable Gigabit mode (full duplex only) for the MAC port specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_GIG=1

Example

       Uint32 portNum = 1;

       CSL_CPGMAC_SL_enableGigabit (portNum);

void CSL_CPGMAC_SL_disableGigabit ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_disableGigabit

Description
This function configures the MAC control register to disable Gigabit mode for MAC port specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_GIG=0

Example

       Uint32 portNum = 1;

       CSL_CPGMAC_SL_disableGigabit (portNum);

Uint32 CSL_CPGMAC_SL_isTxShortGapEnabled ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_isTxShortGapEnabled

Description
This function indicates if Transmit short gap is enabled in the MAC control register for the MAC port specified.

Arguments

       portNum                 MAC port number for which the API must
                               retrieve the settings.
*    

Return Value
TRUE Transmit short gap with a short IPG enabled
FALSE Transmit short gap disabled.

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_MAC_CONTROL_REG_TX_SHORT_GAP_ENABLE

Example

*      Uint32 portNum  =   1;

       if (CSL_CPGMAC_SL_isTxShortGapEnabled (portNum) == TRUE)
       {
           // Tx short gap enabled
       }
       else
       {
           // Tx short gap disabled
       }

void CSL_CPGMAC_SL_enableTxShortGap ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_enableTxShortGap

Description
This function configures the MAC control register to enable transmit short gap for MAC port specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_TX_SHORT_GAP_ENABLE=1

Example

       Uint32 portNum  =   1;

       CSL_CPGMAC_SL_enableTxShortGap (portNum);

void CSL_CPGMAC_SL_disableTxShortGap ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_disableTxShortGap

Description
This function configures the MAC control register to disable transmit short gap for the MAC port specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_TX_SHORT_GAP_ENABLE=0

Example

       Uint32 portNum  =   1;

       CSL_CPGMAC_SL_disableTxShortGap (portNum);

Uint32 CSL_CPGMAC_SL_isIdleModeEnabled ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_isIdleModeEnabled

Description
This function indicates if Idle mode is enabled in the MAC control register for MAC port specified.

Arguments

       portNum                 MAC port number for which the API must
                               retrieve the settings.
*    

Return Value
TRUE Idle mode enabled
FALSE Idle mode disabled.

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_MAC_CONTROL_REG_CMD_IDLE

Example

*      Uint32  portNum = 1;

       if (CSL_CPGMAC_SL_isTxShortGapEnabled (portNum) == TRUE)
       {
           // idle mode enabled
       }
       else
       {
           // idle mode disabled
       }

void CSL_CPGMAC_SL_enableIdleMode ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_enableIdleMode

Description
This function configures the MAC control register to enable Idle mode for MAC port specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_CMD_IDLE=1

Example

       Uint32 portNum  =   1;

       CSL_CPGMAC_SL_enableIdleMode (portNum);

void CSL_CPGMAC_SL_disableIdleMode ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_disableIdleMode

Description
This function configures the MAC control register to disable Idle mode for MAC port specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_CMD_IDLE=0

Example

       Uint32 portNum = 1;

       CSL_CPGMAC_SL_disableIdleMode (portNum);

Uint32 CSL_CPGMAC_SL_isCastagnoliCRCEnabled ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_isCastagnoliCRCEnabled

Description
This function indicates if Castagnoli CRC is enabled in the MAC control register for MAC port specified.

Arguments

       portNum                 MAC port number for which the API must
                               retrieve the settings.
*    

Return Value
TRUE Castagnoli CRC enabled
FALSE Castagnoli CRC disabled.

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_MAC_CONTROL_REG_CRC_TYPE

Example

*      Uint32  portNum = 1;

       if (CSL_CPGMAC_SL_isTxShortGapEnabled (portNum) == TRUE)
       {
           // idle mode enabled
       }
       else
       {
           // idle mode disabled
       }

void CSL_CPGMAC_SL_enableCastagnoliCRC ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_enableCastagnoliCRC

Description
This function configures the MAC control register to enable Castagnoli CRC for MAC port specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_CRC_TYPE=1

Example

       Uint32 portNum  =   1;

       CSL_CPGMAC_SL_enableCastagnoliCRC (portNum);

void CSL_CPGMAC_SL_disableCastagnoliCRC ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_disableCastagnoliCRC

Description
This function configures the MAC control register to disable Castagnoli CRC for MAC port specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_CRC_TYPE=0

Example

       Uint32 portNum = 1;

       CSL_CPGMAC_SL_disableCastagnoliCRC (portNum);

Uint32 CSL_CPGMAC_SL_isIFCTLAEnabled ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_isIFCTLAEnabled

Description
This function indicates if IFCTL_A bit is set in the MAC control register for MAC port specified.

Arguments

       portNum                 MAC port number for which the API must
                               retrieve the settings.
*    

Return Value
TRUE IFCTL_A bit in MAC control register is set to 1.
FALSE IFCTL_A bit in MAC control register reads 0.

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_MAC_CONTROL_REG_IFCTL_A

Example

*      Uint32 portNum  =   1;

       if (CSL_CPGMAC_SL_isIFCTLAEnabled (portNum) == TRUE)
       {
           // IFCTL_A bit set
       }
       else
       {
           // IFCTL_A bit cleared
       }

void CSL_CPGMAC_SL_enableIFCTLA ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_enableIFCTLA

Description
This function enables the IFCTL_A bit in the MAC control register for MAC port number specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_IFCTL_A=1

Example

       Uint32 portNum  =   1;

       CSL_CPGMAC_SL_enableIFCTLA (portNum);

void CSL_CPGMAC_SL_disableIFCTLA ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_disableIFCTLA

Description
This function configures the MAC control register to clear the IFCTL_A bit for MAC port number specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_IFCTL_A=0

Example

       Uint32  portNum =   1;

       CSL_CPGMAC_SL_disableIFCTLA (portNum);

Uint32 CSL_CPGMAC_SL_isIFCTLBEnabled ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_isIFCTLBEnabled

Description
This function indicates if IFCTL_B bit is set in the MAC control register for the MAC port number specified.

Arguments

       portNum                 MAC port number for which the API must
                               retrieve the settings.
*    

Return Value
TRUE IFCTL_B bit in MAC control register is set to 1.
FALSE IFCTL_B bit in MAC control register reads 0.

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_MAC_CONTROL_REG_IFCTL_B

Example

       Uint32  portNum =   1;

       if (CSL_CPGMAC_SL_isIFCTLBEnabled (portNum) == TRUE)
       {
           // IFCTL_B bit set
       }
       else
       {
           // IFCTL_B bit cleared
       }

void CSL_CPGMAC_SL_enableIFCTLB ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_enableIFCTLB

Description
This function enables the IFCTL_B bit in the MAC control register for the MAC port number specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_IFCTL_B=1

Example

       Uint32  portNum =   1;

       CSL_CPGMAC_SL_enableIFCTLB (portNum);

void CSL_CPGMAC_SL_disableIFCTLB ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_disableIFCTLB

Description
This function configures the MAC control register to clear the IFCTL_B bit for the MAC port number specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_IFCTL_B=0

Example

       Uint32 portNum = 1;

       CSL_CPGMAC_SL_disableIFCTLB (portNum);

Uint32 CSL_CPGMAC_SL_isGigForceModeEnabled ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_isGigForceModeEnabled

Description
This function indicates if Gigabit mode force bit is enabled in the MAC control register for the MAC port number specified.

Arguments

       portNum                 MAC port number for which the API must
                               retrieve the settings.
*    

Return Value
TRUE Gigabit mode force enabled.
FALSE Gigabit mode force disabled.

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_MAC_CONTROL_REG_GIG_FORCE

Example

       Uint32  portNum =   1;

       if (CSL_CPGMAC_SL_isGigForceModeEnabled (portNum) == TRUE)
       {
           // gig mode force enabled
       }
       else
       {
           // gig mode force disabled
       }

void CSL_CPGMAC_SL_enableGigForceMode ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_enableGigForceMode

Description
This function configures the MAC control register to enable Gigabit force mode for the MAC port number specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_GIG_FORCE=1

Example

       Uint32  portNum =   1;

       CSL_CPGMAC_SL_enableGigForceMode (portNum);

void CSL_CPGMAC_SL_disableGigForceMode ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_disableGigForceMode

Description
This function configures the MAC control register to disable Gigabit force mode for the MAC port number specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_GIG_FORCE=0

Example

       Uint32  portNum =   1;

       CSL_CPGMAC_SL_disableGigForceMode (portNum);

Uint32 CSL_CPGMAC_SL_isExtControlEnabled ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_isExtControlEnabled

Description
This function indicates if EXT_EN bit is enabled in the MAC control register for the MAC port specified. When this bit is set to 1, the Gigabit and Full duplex mode input is taken from an external source and not from the settings configured in this register.

Arguments

       portNum                 MAC port number for which the API must
                               retrieve the settings.
*    

Return Value
TRUE External control mode enabled.
FALSE External control mode disabled.

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_MAC_CONTROL_REG_EXT_EN

Example

*      Uint32  portNum =   1;

       if (CSL_CPGMAC_SL_isExtControlEnabled (portNum) == TRUE)
       {
           // external control mode enabled
       }
       else
       {
           // external control mode disabled
       }

void CSL_CPGMAC_SL_enableExtControl ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_enableExtControl

Description
This function configures the MAC control register to enable external control of the Gigabit and full duplex mode settings.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_EXT_EN=1

Example

       Uint32 portNum  =   1;

       CSL_CPGMAC_SL_enableExtControl (portNum);

void CSL_CPGMAC_SL_disableExtControl ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_disableExtControl

Description
This function configures the MAC control register to disable external control of the Gigabit and full duplex settings.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_EXT_EN=0

Example

       Uint32 portNum  =   1;

       CSL_CPGMAC_SL_disableExtControl (portNum);

Uint32 CSL_CPGMAC_SL_isExtRxFlowEnabled ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_isExtRxFlowEnabled

Description
This function indicates if EXT_RX_FLOW_EN bit is enabled in the MAC control register for the MAC port specified. When this bit is set to 1, the Rx Flow control enable input is taken from an external source and not from the rx_flow_en setting configured in this register.

Arguments

       portNum                 MAC port number for which the API must
                               retrieve the settings.
*    

Return Value
TRUE External Receive Flow control mode enabled.
FALSE External Receive Flow control mode disabled.

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_MAC_CONTROL_REG_EXT_RX_FLOW_EN

Example

*      Uint32  portNum =   0;

       if (CSL_CPGMAC_SL_isExtRxFlowEnabled (portNum) == TRUE)
       {
           // external control mode enabled
       }
       else
       {
           // external control mode disabled
       }

void CSL_CPGMAC_SL_enableExtRxFlow ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_enableExtRxFlow

Description
This function configures the MAC control register to enable external control of the Receive Flow Control settings.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_EXT_RX_FLOW_EN=1

Example

       Uint32 portNum  =   1;

       CSL_CPGMAC_SL_enableExtRxFlow (portNum);

void CSL_CPGMAC_SL_disableExtRxFlow ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_disableExtRxFlow

Description
This function configures the MAC control register to disable external control of the Receive Flow Control settings.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_EXT_RX_FLOW_EN=0

Example

       Uint32 portNum  =   0;

       CSL_CPGMAC_SL_disableExtRxFlow (portNum);

Uint32 CSL_CPGMAC_SL_isExtTxFlowEnabled ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_isExtTxFlowEnabled

Description
This function indicates if EXT_TX_FLOW_EN bit is enabled in the MAC control register for the MAC port specified. When this bit is set to 1, the Tx Flow control enable input is taken from an external source and not from the rx_flow_en setting configured in this register.

Arguments

       portNum                 MAC port number for which the API must
                               retrieve the settings.
*    

Return Value
TRUE External Transmit Flow control mode enabled.
FALSE External Transmit Flow control mode disabled.

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_MAC_CONTROL_REG_EXT_TX_FLOW_EN

Example

*      Uint32  portNum =   0;

       if (CSL_CPGMAC_SL_isExtTxFlowEnabled (portNum) == TRUE)
       {
           // external control mode enabled
       }
       else
       {
           // external control mode disabled
       }

void CSL_CPGMAC_SL_enableExtTxFlow ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_enableExtTxFlow

Description
This function configures the MAC control register to enable external control of the Transmit Flow Control settings.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_EXT_TX_FLOW_EN=1

Example

       Uint32 portNum  =   1;

       CSL_CPGMAC_SL_enableExtTxFlow (portNum);

void CSL_CPGMAC_SL_disableExtTxFlow ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_disableExtTxFlow

Description
This function configures the MAC control register to disable external control of the Transmit Flow Control settings.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_EXT_TX_FLOW_EN=0

Example

       Uint32 portNum  =   0;

       CSL_CPGMAC_SL_disableExtTxFlow (portNum);

Uint32 CSL_CPGMAC_SL_isRxCEFEnabled ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_isRxCEFEnabled

Description
This function indicates if MAC control register is programmed to copy frames containing errors to its memory.

Arguments

       portNum                 MAC port number for which the API must
                               retrieve the settings.
*    

Return Value
TRUE Copy Error frames mode enabled. Error frames will be transferred to memory.
FALSE Copy Error frames mode disabled. Error frames will be filtered.

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_MAC_CONTROL_REG_RX_CEF_EN

Example

*      Uint32  portNum =   1;

       if (CSL_CPGMAC_SL_isRxCEFEnabled (portNum) == TRUE)
       {
           // Rx CEF enabled
       }
       else
       {
           // Rx CEF disabled
       }

void CSL_CPGMAC_SL_enableRxCEF ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_enableRxCEF

Description
This function configures the MAC control register to enable transfer of frames containing errors.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_RX_CEF_EN=1

Example

       Uint32 portNum = 1;

       CSL_CPGMAC_SL_enableRxCEF (portNum);

void CSL_CPGMAC_SL_disableRxCEF ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_disableRxCEF

Description
This function configures the MAC control register to disable any error frames being transferred to the memory.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_RX_CEF_EN=0

Example

       Uint32 portNum = 1;

       CSL_CPGMAC_SL_disableRxCEF (portNum);

Uint32 CSL_CPGMAC_SL_isRxCSFEnabled ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_isRxCSFEnabled

Description
This function indicates if MAC control register is programmed to copy short frames (frames shorter than 64 bytes) to its memory.

Arguments

       portNum                 MAC port number for which the API must
                               retrieve the settings.
*    

Return Value
TRUE Copy Short frames mode enabled. Short frames will be transferred to memory.
FALSE Copy Short frames mode disabled. Short frames will be filtered.

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_MAC_CONTROL_REG_RX_CSF_EN

Example

       Uint32 portNum = 1;

       if (CSL_CPGMAC_SL_isRxCSFEnabled (portNum) == TRUE)
       {
           // Rx CSF enabled
       }
       else
       {
           // Rx CSF disabled
       }

void CSL_CPGMAC_SL_enableRxCSF ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_enableRxCSF

Description
This function configures the MAC control register to enable transfer of frames that are shorter than 64 bytes.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_RX_CSF_EN=1

Example

       Uint32 portNum = 1;

       CSL_CPGMAC_SL_enableRxCSF (portNum);

void CSL_CPGMAC_SL_disableRxCSF ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_disableRxCSF

Description
This function configures the MAC control register to disable any short frames being transferred to the memory.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_RX_CSF_EN=0

Example

       Uint32 portNum = 1;

       CSL_CPGMAC_SL_disableRxCSF (portNum);

Uint32 CSL_CPGMAC_SL_isRxCMFEnabled ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_isRxCMFEnabled

Description
This function indicates if MAC control register is programmed to copy MAC Control Frames to its memory.

Arguments

       portNum                 MAC port number for which the API must
                               retrieve the settings.
*    

Return Value
TRUE Copy MAC control frames mode enabled. MAC control frames will be transferred to memory.
FALSE Copy MAC control frames mode disabled. MAC control frames will be filtered.

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_MAC_CONTROL_REG_RX_CMF_EN

Example

       Uint32 portNum = 1;

       if (CSL_CPGMAC_SL_isRxCMFEnabled (portNum) == TRUE)
       {
           // Rx CMF enabled
       }
       else
       {
           // Rx CMF disabled
       }

void CSL_CPGMAC_SL_enableRxCMF ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_enableRxCMF

Description
This function configures the MAC control register to enable transfer of MAC control frames.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_RX_CMF_EN=1

Example

       Uint32 portNum = 1;

       CSL_CPGMAC_SL_enableRxCMF (portNum);

void CSL_CPGMAC_SL_disableRxCMF ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_disableRxCMF

Description
This function configures the MAC control register to disable any MAC control frames being transferred to the memory.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_CONTROL_REG_RX_CMF_EN=0

Example

       Uint32  portNum =   1;

       CSL_CPGMAC_SL_disableRxCMF (portNum);

Uint32 CSL_CPGMAC_SL_getMacControlReg ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_getMacControlReg

Description
This function retrieves the contents of MAC control register in entirety.

Arguments

       portNum                 MAC port number for which the API must
                               retrieve the settings.
*    

Return Value
>=0 MAC control register contents.

Pre Condition
None

Post Condition
None

Reads
CPGMAC_SL_MACCONTROL_REG

Example

       Uint32          macControlVal, portNum = 1;

       macControlVal   =   CSL_CPGMAC_SL_getMacControlReg (portNum);

void CSL_CPGMAC_SL_setMacControlReg ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum,
Uint32  macControlRegVal 
)

============================================================================
CSL_CPGMAC_SL_setMacControlReg

Description
This function configures the contents of MAC control register in entirety.

Arguments

       portNum             MAC port number for which the reset must be performed.
       macControlRegVal    value to be configured to the MAC control register.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
CPGMAC_SL_MACCONTROL_REG

Example

       Uint32          macControlVal, portNum = 1;

       macControlVal   =   CSL_CPGMAC_SL_getMacControlReg ();

       // Enable full duplex, giagbit mode too
       macControlVal   |=  CSL_CPGMAC_SL_MACCONTROL_FULLDUPLEX_EN |
                           CSL_CPGMAC_SL_MACCONTROL_GMII_EN;

       CSL_CPGMAC_SL_setMacControlReg (macControlVal, portNum);

void CSL_CPGMAC_SL_getMacStatusReg ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum,
CSL_CPGMAC_SL_MACSTATUS pMacStatus 
)

============================================================================
CSL_CPGMAC_SL_getMacStatusReg

Description
This function retrieves the contents of MAC status register.

Arguments

       portNum                 MAC port number for which the API must
                               retrieve the settings.
       pMacStatus              CSL_CPGMAC_SL_MACSTATUS structure to be populated with
                               the contents of MAC status register.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_MAC_STATUS_REG_TX_FLOW_ACT, XGE_CPSW_PN_MAC_STATUS_REG_RX_FLOW_ACT, XGE_CPSW_PN_MAC_STATUS_REG_EXT_FULLDUPLEX, XGE_CPSW_PN_MAC_STATUS_REG_EXT_GIG, XGE_CPSW_PN_MAC_STATUS_REG_EXT_TX_FLOW_EN, XGE_CPSW_PN_MAC_STATUS_REG_EXT_TX_FLOW_EN, XGE_CPSW_PN_MAC_STATUS_REG_IDLE

Example

       CSL_CPGMAC_SL_MACSTATUS      macStatus;
       Uint32                       portNum = 1;

       CSL_CPGMAC_SL_getMacStatusReg (portNum, &macStatus);

void CSL_CPGMAC_SL_resetMac ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_resetMac

Description
This function issues a software reset to the MAC for the MAC port number specified.

Arguments

       portNum             MAC port number for which the reset must be performed.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_SOFT_RESET_REG_SOFT_RESET=1

Example

       Uint32 portNum  =   1;

       CSL_CPGMAC_SL_resetMac (portNum);

Uint32 CSL_CPGMAC_SL_isMACResetDone ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_isMACResetDone

Description
This function reads the MAC Soft Reset register to check if the software reset operation has completed.

Arguments

       portNum                 MAC port number for which the API must
                               retrieve the settings.
*    

Return Value
TRUE MAC Soft reset done.
FALSE MAC Soft reset not yet completed.

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_MAC_SOFT_RESET_REG_SOFT_RESET

Example

       Uint32  portNum = 1;

       CSL_CPGMAC_SL_resetMac (portNum);

       // Wait until MAC software reset completes
       while (!CSL_CPGMAC_SL_isMACResetDone (portNum));

Uint32 CSL_CPGMAC_SL_getRxMaxLen ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_getRxMaxLen

Description
This function retrieves the Receive maximum frame length configured in Receive Maximum length register for the MAC port number specified.

Arguments

       portNum                 MAC port number for which the API must
                               retrieve the settings.
*    

Return Value
>=0 Receive maximum frame length read.

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_RX_MAXLEN_REG_RX_MAXLEN

Example

       Uint32          mtu, portNum = 1;

       mtu =   CSL_CPGMAC_SL_getRxMaxLen (portNum);

Uint32 CSL_CPGMAC_SL_setRxMaxLen ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum,
Uint32  rxMaxLen 
)

============================================================================
CSL_CPGMAC_SL_setRxMaxLen

Description
This function sets up the Receive maximum frame length in Receive Maximum Length register for the MAC port number specified.

Arguments

       portNum             MAC port number for which the settings must be configured.
       rxMaxLen            the Receive maximum frame length to be configered into
                           the Receive Maximum Length register
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_RX_MAXLEN_REG_RX_MAXLEN

Example

       Uint32          mtu, portNum = 1;

       mtu =   1518;

       CSL_CPGMAC_SL_setRxMaxLen (portNum, mtu);

Uint32 CSL_CPGMAC_SL_getTxGap ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_getTxGap

Description
This function retrieves the Transmit inter-packet gap configured in Transmit Gap register for the MAC port number specified.

Arguments

       portNum                 MAC port number for which the API must
                               retrieve the settings.
*    

Return Value
>=0 Transmit inter-packet gap read.

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_MAC_TX_GAP_REG_TX_GAP

Example

       Uint32          txGap, portNum = 0;

       txGap =   CSL_CPGMAC_SL_getTxGap (portNum);

Uint32 CSL_CPGMAC_SL_setTxGap ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum,
Uint32  txGap 
)

============================================================================
CSL_CPGMAC_SL_setTxGap

Description
This function sets up the Transmit inter-packet gap in Transmit Gap register for the MAC port number specified.

Arguments

       portNum             MAC port number for which the settings must be configured.
       txGap               Transmit inter-packet gap to be configured into the
                           Tx Gap register
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_TX_GAP_REG_TX_GAP

Example

       Uint32          txGap, portNum = 1;

       txGap =   100;

       CSL_CPGMAC_SL_setTxGap (portNum, txGap);

Uint32 CSL_CPGMAC_SL_getRxPauseTimerReg ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_getRxPauseTimerReg

Description
This function retrieves the Receive pause timer value configured in Receive pause timer register for the MAC port specified.

Arguments

       portNum                 MAC port number for which the API must
                               retrieve the settings.
*    

Return Value
>=0 Receive pause timer value read.

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_MAC_RX_PAUSETIMER_REG_RX_PAUSETIMER

Example

       Uint32          rxPauseTimer, portNum = 1;

       rxPauseTimer =   CSL_CPGMAC_SL_getRxPauseTimerReg (portNum);

Uint32 CSL_CPGMAC_SL_setRxPauseTimerReg ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum,
Uint32  rxPauseTimer 
)

============================================================================
CSL_CPGMAC_SL_setRxPauseTimerReg

Description
This function sets up the Receive pause timer value in Receive pause timer register for the MAC port specified.

Arguments

       portNum             MAC port number for which the settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_RX_PAUSETIMER_REG_RX_PAUSETIMER

Example

       Uint32          rxPauseTimer = 2, portNum = 1;

       CSL_CPGMAC_SL_setRxPauseTimerReg (portNum, rxPauseTimer);

Uint32 CSL_CPGMAC_SL_getTxPauseTimerReg ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_getTxPauseTimerReg

Description
This function retrieves the Transmit pause timer value configured in Transmit pause timer register for the MAC port specified.

Arguments

       portNum                 MAC port number for which the API must
                               retrieve the settings.
*    

Return Value
>=0 Transmit pause timer value read.

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_MAC_TX_PAUSETIMER_REG_TX_PAUSETIMER

Example

       Uint32          txPauseTimer, portNum = 1;

       txPauseTimer =   CSL_CPGMAC_SL_getTxPauseTimerReg (portNum);

Uint32 CSL_CPGMAC_SL_setTxPauseTimerReg ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum,
Uint32  txPauseTimer 
)

============================================================================
CSL_CPGMAC_SL_setTxPauseTimerReg

Description
This function sets up the Transmit pause timer value in Transmit pause timer register for the MAC port number specified.

Arguments

       portNum             MAC port number for which the settings must be configured.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_MAC_TX_PAUSETIMER_REG_TX_PAUSETIMER

Example

       Uint32          txPauseTimer = 2, portNum = 1;

       CSL_CPGMAC_SL_setTxPauseTimerReg (portNum, txPauseTimer);

void CSL_CPGMAC_SL_getEmulControlReg ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum,
Uint32 *  pEmulFreeBit,
Uint32 *  pEmulSoftBit 
)

============================================================================
CSL_CPGMAC_SL_getEmulControlReg

Description
This function retrieves the contents of Emulation control register for the MAC port number specified.

Arguments

       portNum             MAC port number for which the API should retrieve
                           emulation settings for.
       pEmulFreeBit        Emulation free bit.
       pEmulSoftBit        Emulation soft bit.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_MAC_EMCONTROL_REG_FREE, XGE_CPSW_PN_MAC_EMCONTROL_REG_SOFT

Example

       Uint32          emulSoftBit, emulFreeBit, portNum = 1;

       CSL_CPGMAC_SL_getEmulControlReg (portNum, &emulFreeBit, &emulSoftBit);

void CSL_CPGMAC_SL_setEmulControlReg ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum,
Uint32  emulFreeBit,
Uint32  emulSoftBit 
)

============================================================================
CSL_CPGMAC_SL_setEmulControlReg

Description
This function sets up the contents of Emulation control register for the MAC port specified.

Arguments

       portNum             MAC port for which the settings must be configured.
       emulFreeBit         Emulation free bit.
       emulSoftBit         Emulation soft bit.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Reads
XGE_CPSW_PN_MAC_EMCONTROL_REG_FREE, XGE_CPSW_PN_MAC_EMCONTROL_REG_SOFT

Example

       Uint32          emulSoftBit, emulFreeBit, portNum = 1;

       emulFreeBit =   1;
       emulSoftBit =   0;

       CSL_CPGMAC_SL_setEmulControlReg (portNum, emulFreeBit, emulSoftBit);

void CSL_CPGMAC_SL_getMacRxPriMapReg ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum,
Uint32 *  pMacRxPriMap 
)

============================================================================
CSL_CPGMAC_SL_getMacRxPriMapReg

Description
This function retrieves the contents of the MAC Receive Packet Priority to Header Priority Mapping Register for the MAC port specified.

Arguments

       portNum                 MAC port number for which the API should retrieve
                               settings for.
       pMacRxPriMap            Array of MAC Rx packet priority map priority values
                               read from the register.
*    

Return Value
None

Pre Condition
The input parameter 'pMacRxPriMap' must be large enough to hold all the 8 priority values read from the register.

Post Condition
None

Reads
XGE_CPSW_PN_RX_PRI_MAP_REG_PRI0, XGE_CPSW_PN_RX_PRI_MAP_REG_PRI1, XGE_CPSW_PN_RX_PRI_MAP_REG_PRI2, XGE_CPSW_PN_RX_PRI_MAP_REG_PRI3, XGE_CPSW_PN_RX_PRI_MAP_REG_PRI4, XGE_CPSW_PN_RX_PRI_MAP_REG_PRI5, XGE_CPSW_PN_RX_PRI_MAP_REG_PRI6, XGE_CPSW_PN_RX_PRI_MAP_REG_PRI7

Example

*      Uint32      pPortRxPriMap [8], portNum = 1;

       CSL_CPGMAC_SL_getMacRxPriMapReg (portNum, pPortRxPriMap);

void CSL_CPGMAC_SL_setMacRxPriMapReg ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum,
Uint32 *  pMacRxPriMap 
)

============================================================================
CSL_CPGMAC_SL_setMacRxPriMapReg

Description
This function sets up the contents of the MAC Receive Packet Priority to Header Priority Mapping Register for the MAC port specified.

Arguments

       portNum                 MAC port for which the settings must be configured.
       pMacRxPriMap            Array of MAC Rx priority map priority values
                               that must be configured to the register.
*    

Return Value
None

Pre Condition
None

Post Condition
None

Writes
XGE_CPSW_PN_RX_PRI_MAP_REG_PRI0, XGE_CPSW_PN_RX_PRI_MAP_REG_PRI1, XGE_CPSW_PN_RX_PRI_MAP_REG_PRI2, XGE_CPSW_PN_RX_PRI_MAP_REG_PRI3, XGE_CPSW_PN_RX_PRI_MAP_REG_PRI4, XGE_CPSW_PN_RX_PRI_MAP_REG_PRI5, XGE_CPSW_PN_RX_PRI_MAP_REG_PRI6, XGE_CPSW_PN_RX_PRI_MAP_REG_PRI7

Example

*      Uint32      i, pMacRxPriMap [8], portNum = 1;

       for (i = 0; i < 8; i ++)
           pMacRxPriMap [i] = i;

       CSL_CPGMAC_SL_setMacRxPriMapReg (portNum, pMacRxPriMap);

void CSL_CPGMAC_SL_clearMacStatusTorf ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_clearMacStatusTorf

Description
This function clears Top of receive FIFO flow control trigger bit in PN_MAC_STATUS register

Arguments

       portNum                 MAC port number
*    

Return Value
None

Pre Condition
None

Post Condition
None


void CSL_CPGMAC_SL_clearMacStatusTorfPri ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_clearMacStatusTorf

Description
This function clears Top of receive FIFO flow control Priority field in PN_MAC_STATUS register

Arguments

       portNum                 MAC port number
*    

Return Value
None

Pre Condition
None

Post Condition
None


void CSL_CPGMAC_SL_getInterVLANCfg ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum,
Uint32  routeIndex,
CSL_CPSW_INTERVLANCFG pInterVLANCfg 
)

============================================================================
CSL_CPGMAC_SL_getInterVLANCfg

Description
This function gets the intervlan configuration for the given port and route index

Arguments

*       portNum   Port number for which the intervlan configuration is queried
*       routeIndex Intervlan route index.Valid pointer locations are 1 to x
*                  (where x is the number of locations - pointer location zero
*                   is unused).
*       pInterVLANCfg Intervlan configuration structure to be populated
*   

Return Value
none


void CSL_CPGMAC_SL_setInterVLANCfg ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum,
Uint32  routeIndex,
CSL_CPSW_INTERVLANCFG pInterVLANCfg 
)

============================================================================
CSL_CPGMAC_SL_setInterVLANCfg

Description
This function sets the intervlan configuration for the given port and route index

Arguments

*       portNum   Port number for which the intervlan configuration is queried
*       routeIndex Intervlan route index.Valid pointer locations are 1 to x
*                  (where x is the number of locations - pointer location zero
*                   is unused).
*       pInterVLANCfg Intervlan configuration structure to be set
*   

Return Value
none


void CSL_CPGMAC_SL_getFifoStatus ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum,
CSL_CPGMAC_SL_FIFOSTATUS pFifoStatus 
)

============================================================================
CSL_CPGMAC_SL_getFifoStatus

Description
This function gets the Enet_Pn_FIFO_Status register contents

Arguments

*       portNum   Port number for which the intervlan configuration is queried
*       pFifoStatus Fifo status structure to be populated
*   

Return Value
none


Uint32 CSL_CPGMAC_SL_isTxShortGapLimitEnabled ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_isTxShortGapLimitEnabled

Description
This function indicates if Transmit short gap limit is enabled in the MAC control register for the MAC port specified. When set this bit limits the number of short gap packets transmitted to 100ppm. Each time a short gap packet is sent, a counter is loaded with 10,000 and decremented on each wireside clock. Another short gap packet will not be sent out until the counter decrements to zero. This mode is included to preclude the host from filling up the FIFO and sending every packet out with short gap which would violate the maximum number of packets per second allowed. This bit is used only with GMII (not XGMII).

Arguments

       portNum                 MAC port number for which the API must
                               retrieve the settings.
*    

Return Value
TRUE Transmit short gap limit with a short IPG enabled
FALSE Transmit short gap limit disabled.


void CSL_CPGMAC_SL_enableTxShortGapLimit ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_enableTxShortGap

Description
This function configures the MAC control register to enable transmit short gap limiting for MAC port specified. When set this bit limits the number of short gap packets transmitted to 100ppm. Each time a short gap packet is sent, a counter is loaded with 10,000 and decremented on each wireside clock. Another short gap packet will not be sent out until the counter decrements to zero. This mode is included to preclude the host from filling up the FIFO and sending every packet out with short gap which would violate the maximum number of packets per second allowed. This bit is used only with GMII (not XGMII).

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None


void CSL_CPGMAC_SL_disableTxShortGapLimit ( CSL_Xge_cpswRegs *  hCpswRegs,
Uint32  portNum 
)

============================================================================
CSL_CPGMAC_SL_disableTxShortGapLimit

Description
This function configures the MAC control register to disable transmit short gap limit for the MAC port specified.

Arguments

       portNum                 MAC port number for which settings must be configured.
*    

Return Value
None