![]() |
PDK API Guide for AM65xx
|
Functions | |
| void | CpswUtils_checkPktState (uint32_t *pStateVar, CpswUtils_PktStateModuleType module, uint32_t expectedState, uint32_t newState) |
| Packet state check & set API for app, memory manager and dma driver. More... | |
| void | CpswUtils_checkDescState (uint32_t *pStateVar, CpswUtils_DescStateMemMgr expectedState, CpswUtils_DescStateMemMgr newState) |
| Descriptor state check & set API for descriptor memory manager. More... | |
Enumerations | |
| enum | CpswUtils_DescStateMemMgr { CPSW_DESCSTATE_MEMMGR_FREE = 0U, CPSW_DESCSTATE_MEMMGR_ALLOC } |
| CPSW DMA Descriptor state. More... | |
| enum | CpswUtils_PktStateApp { CPSW_PKTSTATE_APP_WITH_FREEQ = 0U, CPSW_PKTSTATE_APP_WITH_READYQ, CPSW_PKTSTATE_APP_WITH_DRIVER } |
| App Pkt state. More... | |
| enum | CpswUtils_PktStateDma { CPSW_PKTSTATE_DMA_WITH_HW = 0U, CPSW_PKTSTATE_DMA_NOT_WITH_HW } |
| DMA Pkt state. More... | |
| enum | CpswUtils_PktStateMemMgr { CPSW_PKTSTATE_MEMMGR_FREE = 0U, CPSW_PKTSTATE_MEMMGR_ALLOC } |
| CPSW DMA Pkt state. More... | |
| enum | CpswUtils_PktStateModuleType { CPSW_PKTSTATE_MODULE_APP = 0U, CPSW_PKTSTATE_MODULE_DRIVER, CPSW_PKTSTATE_MODULE_MEMUTILS } |
| CPSW DMA Pkt state. More... | |
Macros | |
| #define | CPSW_UTILS_GET_STATE(state, mask, bitshift) |
| #define | CPSW_UTILS_SET_STATE(state, mask, bitshift, value) |
| #define | CPSW_UTILS_DRIVER_STATE_MASK (0x000000FFU) |
| #define | CPSW_UTILS_DRIVER_STATE_BIT_SHIFT (0U) |
| #define | CPSW_UTILS_MEMUTILS_STATE_MASK (0x0000FF00U) |
| #define | CPSW_UTILS_MEMUTILS_STATE_BIT_SHIFT (8U) |
| #define | CPSW_UTILS_APP_STATE_MASK (0x00FF0000U) |
| #define | CPSW_UTILS_APP_STATE_BIT_SHIFT (16U) |
| #define | CPSW_UTILS_GET_PKT_DRIVER_STATE(state) |
| #define | CPSW_UTILS_SET_PKT_DRIVER_STATE(state, value) |
| #define | CPSW_UTILS_GET_PKT_MEMUTILS_STATE(state) |
| #define | CPSW_UTILS_SET_PKT_MEMUTILS_STATE(state, value) |
| #define | CPSW_UTILS_GET_PKT_APP_STATE(state) |
| #define | CPSW_UTILS_SET_PKT_APP_STATE(state, value) |
| #define | CPSW_UTILS_MEMUTILS_DESCSTATE_MASK (0x000000FFU) |
| #define | CPSW_UTILS_MEMUTILS_DESCSTATE_SHIFT (0U) |
| #define | CPSW_UTILS_GET_DESC_MEMUTILS_STATE(state) |
| #define | CPSW_UTILS_SET_DESC_MEMUTILS_STATE(state, value) |
| #define CPSW_UTILS_GET_STATE | ( | state, | |
| mask, | |||
| bitshift | |||
| ) |
| #define CPSW_UTILS_SET_STATE | ( | state, | |
| mask, | |||
| bitshift, | |||
| value | |||
| ) |
| #define CPSW_UTILS_DRIVER_STATE_MASK (0x000000FFU) |
| #define CPSW_UTILS_DRIVER_STATE_BIT_SHIFT (0U) |
| #define CPSW_UTILS_MEMUTILS_STATE_MASK (0x0000FF00U) |
| #define CPSW_UTILS_MEMUTILS_STATE_BIT_SHIFT (8U) |
| #define CPSW_UTILS_APP_STATE_MASK (0x00FF0000U) |
| #define CPSW_UTILS_APP_STATE_BIT_SHIFT (16U) |
| #define CPSW_UTILS_GET_PKT_DRIVER_STATE | ( | state | ) |
| #define CPSW_UTILS_SET_PKT_DRIVER_STATE | ( | state, | |
| value | |||
| ) |
| #define CPSW_UTILS_GET_PKT_MEMUTILS_STATE | ( | state | ) |
| #define CPSW_UTILS_SET_PKT_MEMUTILS_STATE | ( | state, | |
| value | |||
| ) |
| #define CPSW_UTILS_GET_PKT_APP_STATE | ( | state | ) |
| #define CPSW_UTILS_SET_PKT_APP_STATE | ( | state, | |
| value | |||
| ) |
| #define CPSW_UTILS_MEMUTILS_DESCSTATE_MASK (0x000000FFU) |
| #define CPSW_UTILS_MEMUTILS_DESCSTATE_SHIFT (0U) |
| #define CPSW_UTILS_GET_DESC_MEMUTILS_STATE | ( | state | ) |
| #define CPSW_UTILS_SET_DESC_MEMUTILS_STATE | ( | state, | |
| value | |||
| ) |
| void CpswUtils_checkPktState | ( | uint32_t * | pStateVar, |
| CpswUtils_PktStateModuleType | module, | ||
| uint32_t | expectedState, | ||
| uint32_t | newState | ||
| ) |
Packet state check & set API for app, memory manager and dma driver.
This development time API checks expected state and sets new packet state. This is used by modules handling the packet to confirm the packet is returned and allocated in correct state. Memutils checks (free, allocated), dma driver checks (with Hw, with driver) and app checks which Q it belongs
| pStateVar | [IN/OUT] Pointer to packet state variable of packet structure CpswDma_PktInfo |
| module | [IN] Module id. Refer to CpswUtils_PktStateModuleType |
| expectedState | [IN] State packet is expected to be. |
| newState | [IN] New state packet is set to. |
| void CpswUtils_checkDescState | ( | uint32_t * | pStateVar, |
| CpswUtils_DescStateMemMgr | expectedState, | ||
| CpswUtils_DescStateMemMgr | newState | ||
| ) |
Descriptor state check & set API for descriptor memory manager.
This development time API checks expected state and sets new descriptor state. This is used by modules handling the Desc to confirm the Desc is returned and allocated in correct state. Only memutils modules uses it now for checking if desc is free or allocated while allocating or freeing desc respectively.
| pStateVar | [IN/OUT] Pointer to Desc state variable. |
| expectedState | [IN] State Desc is expected to be. |
| newState | [IN] New state Desc is set to. |