PDK API Guide for AM65xx

Introduction

Application interfaces provided by TPS65941 PMIC device library.

Data Structures

struct  Board_Tps65941GpioRegCfg
 TPS65941 gpio details object structure. More...
 
struct  Board_Tps65941PwrResourceRegCfg
 TPS65941 power resource details object structure. More...
 
struct  Board_Tps65941IntrRegMap
 TPS65941 power resource details object structure. More...
 
struct  Board_Tps65941VoltMonitorCfg
 TPS65941 voltage monitoring details object structure. More...
 
struct  Board_Tps65941RtcTime
 TPS65941 RTC time object structure. More...
 
struct  Board_Tps65941RtcDate
 TPS65941 RTC Date object structure. More...
 
struct  Board_Tps65941WdtCfg
 TPS65941 WDT configuration parameters object structure. More...
 
struct  Board_Tps65941EsmCfg
 TPS65941 ESM configuration parameters object structure. More...
 

Functions

Board_STATUS Board_tps65941GpioRead (void *handle, uint8_t slaveAddr, uint8_t pinNum, uint8_t *pinValue)
 TPS65941 GPIO read function. More...
 
Board_STATUS Board_tps65941GpioWrite (void *handle, uint8_t slaveAddr, uint8_t pinNum, uint8_t pinValue)
 TPS65941 GPIO write function. More...
 
Board_STATUS Board_tps65941SetVoltage (void *handle, uint8_t slaveAddr, uint8_t powerResource, uint16_t millivolt)
 TPS65941 set voltage function. More...
 
Board_STATUS Board_tps65941GetVoltage (void *handle, uint8_t slaveAddr, uint8_t powerResource, uint16_t *millivolt)
 TPS65941 read voltage function. More...
 
Board_STATUS Board_tps65941ConvertVolt (uint8_t voutCode, uint8_t powerResource, uint16_t *millivolt)
 Conversion of VOUT code to millivolt. More...
 
Board_STATUS Board_tps65941ConvertVoutCode (uint16_t millivolt, uint8_t powerResource, uint8_t *voutCode)
 Conversion of millivolt to VOUT code. More...
 
Board_STATUS Board_tps65941ConfigIntr (void *handle, uint8_t slaveAddr, uint32_t intrID, uint8_t intrEnable)
 TPS65941 enable/disable interrupt function. More...
 
Board_STATUS Board_tps65941GetIntrStatus (void *handle, uint8_t slaveAddr, uint32_t intrID, uint8_t *intrStatus)
 Get the TPS65941 interrupt function. More...
 
Board_STATUS Board_tps65941ClearIntr (void *handle, uint8_t slaveAddr, uint32_t intrID)
 Clears the TPS65941 interrupt function. More...
 
Board_STATUS Board_tps65941SetThermalThresVal (void *handle, uint8_t slaveAddr, uint32_t thermalThresholdVal)
 Set the TPS65941 thermal threshold value function. More...
 
Board_STATUS Board_tps65941GetThermalStatus (void *handle, uint8_t slaveAddr, uint32_t *thermalStatus)
 Get the TPS65941 thermal status function. More...
 
Board_STATUS Board_tps65941SetThermalMonitor (void *handle, uint8_t slaveAddr)
 Set the thermal monitoring function. More...
 
Board_STATUS Board_tps65941SetVoltageMonitor (void *handle, uint8_t slaveAddr, uint8_t powerResource, Board_Tps65941VoltMonitorCfg *voltMonCfg)
 Set the voltage monitoring function. More...
 
Board_STATUS Board_tps65941SetVccaMonitor (void *handle, uint8_t slaveAddr, uint8_t vccaPgLevel, Board_Tps65941VoltMonitorCfg *voltMonitorCfg)
 Set the Vcca voltage monitoring function. More...
 
Board_STATUS Board_tps65941SetRtc (void *handle, uint8_t slaveAddr, Board_Tps65941RtcTime *timeCfg, Board_Tps65941RtcDate *dateCfg)
 Set the TPS65941 RTC date and time function. More...
 
Board_STATUS Board_tps65941GetRtc (void *handle, uint8_t slaveAddr, Board_Tps65941RtcTime *timeCfg, Board_Tps65941RtcDate *dateCfg)
 Get the TPS65941 RTC date and time function. More...
 
Board_STATUS Board_tps65941SetAlarmIntr (void *handle, uint8_t slaveAddr, Board_Tps65941RtcTime *timeCfg, Board_Tps65941RtcDate *dateCfg)
 Set the alarm interrupt in TPS65941 RTC function. More...
 
Board_STATUS Board_tps65941SetTimerIntr (void *handle, uint8_t slaveAddr, uint8_t timerPeriod)
 Set the timer interrupt in TPS65941 RTC function. More...
 
Board_STATUS Board_tps65941WdtDisable (void *handle, uint8_t slaveAddr, uint8_t wdtDisable)
 Enable/Disable the TPS65941 Watchdog function. More...
 
Board_STATUS Board_tps65941WdtConfig (void *handle, uint8_t slaveAddr, uint8_t wdtCfgMode, Board_Tps65941WdtCfg *wdtCfg)
 TPS65941 watchdog configuration function. More...
 
Board_STATUS Board_tps65941GetWdtStat (void *handle, uint8_t slaveAddr, uint8_t wdtErrType, uint8_t *wdtErrStat)
 TPS65941 watchdog error status function. More...
 
Board_STATUS Board_tps65941StartEsm (void *handle, uint8_t slaveAddr, uint8_t esmCfg, uint8_t esmMode)
 Start TPS65941 ESM function. More...
 
Board_STATUS Board_tps65941StopEsm (void *handle, uint8_t slaveAddr, uint8_t esmCfg)
 Stop TPS65941 ESM function. More...
 
Board_STATUS Board_tps65941ConfigEsm (void *handle, uint8_t slaveAddr, uint8_t esmCfgType, Board_Tps65941EsmCfg *esmCfg)
 TPS65941 ESM configuration function. More...
 
Board_STATUS Board_tps65941GetEsmCount (void *handle, uint8_t slaveAddr, uint8_t esmCfg, uint8_t *esmErrCnt)
 Get the ESM error count function. More...
 

Function Documentation

Board_STATUS Board_tps65941GpioRead ( void *  handle,
uint8_t  slaveAddr,
uint8_t  pinNum,
uint8_t *  pinValue 
)

TPS65941 GPIO read function.

This function is used to read the gpio signal level of the TPS65941 device.

Parameters
handle[IN] Low level driver handle
slaveAddr[IN] TPS65941 slave address
pinNum[IN] TPS65941 GPIO number
pinValue[OUT] TPS65941 GPIO signal level High/Low
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_tps65941GpioWrite ( void *  handle,
uint8_t  slaveAddr,
uint8_t  pinNum,
uint8_t  pinValue 
)

TPS65941 GPIO write function.

This function is used to write the gpio signal level to the TPS65941 device.

Parameters
handle[IN] Low level driver
slaveAddr[IN] TPS65941 slave address
pinNum[IN] TPS65941 GPIO number
pinValue[IN] TPS65941 GPIO signal level High/Low Valid values: BOARD_TPS65941_GPIO_HIGH BOARD_TPS65941_GPIO_LOW
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_tps65941SetVoltage ( void *  handle,
uint8_t  slaveAddr,
uint8_t  powerResource,
uint16_t  millivolt 
)

TPS65941 set voltage function.

This function is used to set the voltage to the power resource of the TPS65941.

Parameters
handle[IN] Low level driver handle
slaveAddr[IN] TPS65941 slave address
powerResource[IN] TPS65941 Power resource Valid values: BOARD_TPS65941_BUCK1_RESOURCE BOARD_TPS65941_BUCK2_RESOURCE BOARD_TPS65941_BUCK3_RESOURCE BOARD_TPS65941_BUCK4_RESOURCE BOARD_TPS65941_BUCK5_RESOURCE BOARD_TPS65941_LDO1_RESOURCE BOARD_TPS65941_LDO2_RESOURCE BOARD_TPS65941_LDO3_RESOURCE BOARD_TPS65941_LDO4_RESOURCE
millivolt[IN] Voltage in millivolt
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_tps65941GetVoltage ( void *  handle,
uint8_t  slaveAddr,
uint8_t  powerResource,
uint16_t *  millivolt 
)

TPS65941 read voltage function.

This function is used to read the voltage to the power resource of the TPS65941.

Parameters
handle[IN] Low level driver handle
slaveAddr[IN] TPS65941 slave address
powerResource[IN] TPS65941 Power resource Valid values: BOARD_TPS65941_BUCK1_RESOURCE BOARD_TPS65941_BUCK2_RESOURCE BOARD_TPS65941_BUCK3_RESOURCE BOARD_TPS65941_BUCK4_RESOURCE BOARD_TPS65941_BUCK5_RESOURCE BOARD_TPS65941_LDO1_RESOURCE BOARD_TPS65941_LDO2_RESOURCE BOARD_TPS65941_LDO3_RESOURCE BOARD_TPS65941_LDO4_RESOURCE
millivolt[OUT] Voltage in millivolt
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_tps65941ConvertVolt ( uint8_t  voutCode,
uint8_t  powerResource,
uint16_t *  millivolt 
)

Conversion of VOUT code to millivolt.

This function is used to convert the VOUT code read from the PMIC registers to millivolt.

Parameters
voutCode[IN] VOUT code in hexadecimal
powerResource[IN] PMIC Power resource Valid values: BOARD_TPS65941_BUCK1_RESOURCE BOARD_TPS65941_BUCK2_RESOURCE BOARD_TPS65941_BUCK3_RESOURCE BOARD_TPS65941_BUCK4_RESOURCE BOARD_TPS65941_BUCK5_RESOURCE BOARD_TPS65941_LDO1_RESOURCE BOARD_TPS65941_LDO2_RESOURCE BOARD_TPS65941_LDO3_RESOURCE BOARD_TPS65941_LDO4_RESOURCE
millivolt[OUT] Voltage in millivolt
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_tps65941ConvertVoutCode ( uint16_t  millivolt,
uint8_t  powerResource,
uint8_t *  voutCode 
)

Conversion of millivolt to VOUT code.

This function is used to convert the millivolt value to VOUT code to write into the TPS65941 registers.

Parameters
millivolt[IN] Voltage in millivolt
powerResource[IN] TPS65941 Power resource Valid values: BOARD_TPS65941_BUCK1_RESOURCE BOARD_TPS65941_BUCK2_RESOURCE BOARD_TPS65941_BUCK3_RESOURCE BOARD_TPS65941_BUCK4_RESOURCE BOARD_TPS65941_BUCK5_RESOURCE BOARD_TPS65941_LDO1_RESOURCE BOARD_TPS65941_LDO2_RESOURCE BOARD_TPS65941_LDO3_RESOURCE BOARD_TPS65941_LDO4_RESOURCE
voutCode[OUT] VOUT code in hexadecimal
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_tps65941ConfigIntr ( void *  handle,
uint8_t  slaveAddr,
uint32_t  intrID,
uint8_t  intrEnable 
)

TPS65941 enable/disable interrupt function.

This function is used to enable/disable the interrupt of the TPS65941.

Parameters
handle[IN] Low level driver handle
slaveAddr[IN] TPS65941 slave address
intrID[IN] TPS65941 Interrupt ID Use the macros BOARD_TPS65941_INTR_ID_XXX
intrEnable[IN] Enable/Disable the interrupt Valid values: BOARD_TPS65941_INTR_ENABLE BOARD_TPS65941_INTR_DISABLE
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_tps65941GetIntrStatus ( void *  handle,
uint8_t  slaveAddr,
uint32_t  intrID,
uint8_t *  intrStatus 
)

Get the TPS65941 interrupt function.

This function is used to get the interrupt status of the TPS65941.

Parameters
handle[IN] Low level driver handle
slaveAddr[IN] TPS65941 slave address
intrID[IN] TPS65941 Interrupt ID Use the macros BOARD_TPS65941_INTR_ID_XXX
intrStatus[OUT] Interrupt status Valid value: BOARD_TPS65941_INTR_SET BOARD_TPS65941_INTR_UNSET
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_tps65941ClearIntr ( void *  handle,
uint8_t  slaveAddr,
uint32_t  intrID 
)

Clears the TPS65941 interrupt function.

This function is used to clear the interrupt of the TPS65941.

Parameters
handle[IN] Low level driver handle
slaveAddr[IN] TPS65941 slave address
intrID[IN] TPS65941 Interrupt ID Use the macros BOARD_TPS65941_INTR_ID_XXX
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_tps65941SetThermalThresVal ( void *  handle,
uint8_t  slaveAddr,
uint32_t  thermalThresholdVal 
)

Set the TPS65941 thermal threshold value function.

This function is used to set the thermal temperature threshold value for the TPS65941.

Parameters
handle[IN] Low level driver handle
slaveAddr[IN] TPS65941 slave address
thermalThresholdVal[IN] Thermal temperature threshold value Valid Values: BOARD_TPS65941_THERMAL_TEMP_120C BOARD_TPS65941_THERMAL_TEMP_130C
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_tps65941GetThermalStatus ( void *  handle,
uint8_t  slaveAddr,
uint32_t *  thermalStatus 
)

Get the TPS65941 thermal status function.

This function is used to read the thermal status of the TPS65941.

Parameters
handle[IN] Low level driver handle
slaveAddr[IN] TPS65941 slave address
thermalStatus[OUT] TPS65941 Thermal status Valid Value: BOARD_TPS65941_TDIE_NO_WARN BOARD_TPS65941_TDIE_WARN BOARD_TPS65941_TDIE_WARN_ORD_SD BOARD_TPS65941_TDIE_WARN_IMM_SD
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_tps65941SetThermalMonitor ( void *  handle,
uint8_t  slaveAddr 
)

Set the thermal monitoring function.

This function is used to set the thermal temperature monitoring function with PGOOD signal.

Parameters
handle[IN] Low level driver handle
slaveAddr[IN] TPS65941 slave address
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_tps65941SetVoltageMonitor ( void *  handle,
uint8_t  slaveAddr,
uint8_t  powerResource,
Board_Tps65941VoltMonitorCfg voltMonCfg 
)

Set the voltage monitoring function.

This function is used to set the voltage monitoring function to the BUCK and LDO power resources with PGOOD signal.

Parameters
handle[IN] Low level driver handle
slaveAddr[IN] TPS65941 slave address
powerResource[IN] TPS65941 Power resource Valid values: BOARD_TPS65941_BUCK1_RESOURCE BOARD_TPS65941_BUCK2_RESOURCE BOARD_TPS65941_BUCK3_RESOURCE BOARD_TPS65941_BUCK4_RESOURCE BOARD_TPS65941_BUCK5_RESOURCE BOARD_TPS65941_LDO1_RESOURCE BOARD_TPS65941_LDO2_RESOURCE BOARD_TPS65941_LDO3_RESOURCE BOARD_TPS65941_LDO4_RESOURCE
voltMonCfg[IN] TPS65941 voltage monitor details
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_tps65941SetVccaMonitor ( void *  handle,
uint8_t  slaveAddr,
uint8_t  vccaPgLevel,
Board_Tps65941VoltMonitorCfg voltMonitorCfg 
)

Set the Vcca voltage monitoring function.

This function is used to set the voltage monitoring function to the Vcca with PGOOD signal.

Parameters
handle[IN] Low level driver handle
slaveAddr[IN] TPS65941 slave address
vccaPgLevel[IN] TPS65941 Vcca Power good level Valid values: BOARD_TPS65941_PG_3V3_LEVEL BOARD_TPS65941_PG_5V_LEVEL
voltMonitorCfg[IN] TPS65941 voltage monitor details
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_tps65941SetRtc ( void *  handle,
uint8_t  slaveAddr,
Board_Tps65941RtcTime timeCfg,
Board_Tps65941RtcDate dateCfg 
)

Set the TPS65941 RTC date and time function.

This function is used to set the date and time parameters in RTC present in the TPS65941.

Parameters
handle[IN] Low level driver handle
slaveAddr[IN] TPS65941 slave address
timeCfg[IN] TPS65941 RTC time configuration
dateCfg[IN] TPS65941 RTC date configuration
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_tps65941GetRtc ( void *  handle,
uint8_t  slaveAddr,
Board_Tps65941RtcTime timeCfg,
Board_Tps65941RtcDate dateCfg 
)

Get the TPS65941 RTC date and time function.

This function is used to get the current date and time parameters in RTC present in the TPS65941.

Parameters
handle[IN] Low level driver handle
slaveAddr[IN] TPS65941 slave address
timeCfg[OUT] TPS65941 RTC time configuration
dateCfg[OUT] TPS65941 RTC date configuration
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_tps65941SetAlarmIntr ( void *  handle,
uint8_t  slaveAddr,
Board_Tps65941RtcTime timeCfg,
Board_Tps65941RtcDate dateCfg 
)

Set the alarm interrupt in TPS65941 RTC function.

This function is used to set the alarm date and time interrupt in RTC present in the TPS65941.

Parameters
handle[IN] Low level driver handle
slaveAddr[IN] TPS65941 slave address
timeCfg[IN] TPS65941 RTC time configuration
dateCfg[IN] TPS65941 RTC date configuration
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_tps65941SetTimerIntr ( void *  handle,
uint8_t  slaveAddr,
uint8_t  timerPeriod 
)

Set the timer interrupt in TPS65941 RTC function.

This function is used to set the timer interrupt in RTC present in the TPS65941.

Parameters
handle[IN] Low level driver handle
slaveAddr[IN] TPS65941 slave address
timerPeriod[IN] Timer interrupt periods Valid values: BOARD_TPS65941_SECOND_INTR_PERIOD BOARD_TPS65941_MINUTE_INTR_PERIOD BOARD_TPS65941_HOUR_INTR_PERIOD BOARD_TPS65941_DAY_INTR_PERIOD
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_tps65941WdtDisable ( void *  handle,
uint8_t  slaveAddr,
uint8_t  wdtDisable 
)

Enable/Disable the TPS65941 Watchdog function.

This function is used to enable/disable the watchdog function in the TPS65941.

Parameters
handle[IN] Low level driver
slaveAddr[IN] TPS65941 slave address
wdtDisable[IN] Enable/Disable the watchdog Valid values: BOARD_TPS65941_WDT_DISABLE BOARD_TPS65941_WDT_ENABLE
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_tps65941WdtConfig ( void *  handle,
uint8_t  slaveAddr,
uint8_t  wdtCfgMode,
Board_Tps65941WdtCfg wdtCfg 
)

TPS65941 watchdog configuration function.

This function is used to configure the watchdog function parameters in the TPS65941 in either trigger mode or Q&A (question and answer) mode.

Parameters
handle[IN] Low level driver handle
slaveAddr[IN] TPS65941 slave address
wdtCfgMode[IN] Watchdog configuration mode Valid values: BOARD_TPS65941_WDT_QA_MODE BOARD_TPS65941_WDT_TRIGGER_MODE
wdtCfg[IN] TPS65941 watchdog configuration
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_tps65941GetWdtStat ( void *  handle,
uint8_t  slaveAddr,
uint8_t  wdtErrType,
uint8_t *  wdtErrStat 
)

TPS65941 watchdog error status function.

This function is used to get the error status from the TPS65941 watchdog.

Parameters
handle[IN] Low level driver handle
slaveAddr[IN] TPS65941 slave address
wdtErrType[IN] TPS65941 Watchdog error type Valid Values: BOARD_TPS65941_WDT_RST_INT BOARD_TPS65941_WDT_FAIL_INT BOARD_TPS65941_WDT_ANSW_ERR BOARD_TPS65941_WDT_SEQ_ERR BOARD_TPS65941_WDT_ANSW_ERLY_ERR BOARD_TPS65941_WDT_TRIG_ERLY_ERR BOARD_TPS65941_WDT_TIMEOUT_ERR BOARD_TPS65941_WDT_LNGWIN_TIMEOUT_ERR
wdtErrStat[OUT] TPS65941 Watchdog error status Valid Values: BOARD_TPS65941_WDT_ERR_LATCHED BOARD_TPS65941_WDT_NO_ERR
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_tps65941StartEsm ( void *  handle,
uint8_t  slaveAddr,
uint8_t  esmCfg,
uint8_t  esmMode 
)

Start TPS65941 ESM function.

This function is used the start the TPS65941 ESM for SoC or MCU in either level or PWM mode.

Parameters
handle[IN] Low level driver handle
slaveAddr[IN] TPS65941 slave address
esmCfg[IN] ESM configuration Valid values: BOARD_TPS65941_ESM_SOC BOARD_TPS65941_ESM_MCU
esmMode[IN] ESM configuration mode Valid values: BOARD_TPS65941_ESM_LEVEL_MODE BOARD_TPS65941_ESM_PWM_MODE
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_tps65941StopEsm ( void *  handle,
uint8_t  slaveAddr,
uint8_t  esmCfg 
)

Stop TPS65941 ESM function.

This function is used the stop the TPS65941 ESM for SoC or MCU.

Parameters
handle[IN] Low level driver handle
slaveAddr[IN] TPS65941 slave address
esmCfg[IN] ESM configuration Valid values: BOARD_TPS65941_ESM_SOC BOARD_TPS65941_ESM_MCU
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_tps65941ConfigEsm ( void *  handle,
uint8_t  slaveAddr,
uint8_t  esmCfgType,
Board_Tps65941EsmCfg esmCfg 
)

TPS65941 ESM configuration function.

This function is used to configure the TPS65941 ESM parameters.

Parameters
handle[IN] Low level driver handle
slaveAddr[IN] TPS65941 slave address
esmCfgType[IN] ESM configuration type Valid values: BOARD_TPS65941_ESM_SOC BOARD_TPS65941_ESM_MCU
esmCfg[IN] TPS65941 ESM configuration
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_tps65941GetEsmCount ( void *  handle,
uint8_t  slaveAddr,
uint8_t  esmCfg,
uint8_t *  esmErrCnt 
)

Get the ESM error count function.

This function is used to get the number error count events for the TPS65941 ESM for SoC or MCU.

Parameters
handle[IN] Low level driver handle
slaveAddr[IN] TPS65941 slave address
esmCfg[IN] ESM configuration Valid values: BOARD_TPS65941_ESM_SOC BOARD_TPS65941_ESM_MCU
esmErrCnt[OUT] TPS65941 ESM error count
Returns
BOARD_SOK in case of success or appropriate error code.