PDK API Guide for AM65xx

Introduction

Application Interfaces provided by DS90UB960 FPD-Link device library.

Functions

Board_STATUS Board_fpdUb960WriteReg (void *handle, uint32_t slaveAddr, uint8_t regAddr, uint8_t regData)
 UB960 register write function. More...
 
Board_STATUS Board_fpdUb960ReadReg (void *handle, uint32_t slaveAddr, uint8_t regAddr, uint8_t *regData)
 UB960 register read fuunction. More...
 
void Board_fpdU960GetI2CAddr (uint8_t *chNum, uint8_t *i2cAddr, uint32_t csiInst)
 Get ub960 i2c address. More...
 
Board_STATUS Board_fpdUb960CfgPG (void *handle, Board_FpdModuleObj *fpdModParams, uint32_t pgType)
 FPD ub960 pattern generation configurations. More...
 
Board_STATUS Board_fpdUb960DesInit (void *handle, Board_FpdModuleObj *fpdModParams)
 Initializes the FPD UB960 module. More...
 
Board_STATUS Board_fpdUb960DesInitFusionBoardTIDA1130 (void *handle, Board_FpdModuleObj *fpdModParams)
 Initializes the FPD UB960 module for OV2775 sensor module. More...
 
Board_STATUS Board_fpdUb960Cfg (void *handle, Board_FpdModuleObj *fpdModParams, Board_I2cRegProgObj *ub960Cfg)
 FPD ub960 configurations. More...
 

Function Documentation

Board_STATUS Board_fpdUb960WriteReg ( void *  handle,
uint32_t  slaveAddr,
uint8_t  regAddr,
uint8_t  regData 
)

UB960 register write function.

Parameters
handle[IN] I2C driver handle
slaveAddr[IN] Device slave address
regAddr[IN] Register offset address
regData[IN] Register data
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_fpdUb960ReadReg ( void *  handle,
uint32_t  slaveAddr,
uint8_t  regAddr,
uint8_t *  regData 
)

UB960 register read fuunction.

Parameters
handle[IN] I2C driver handle
slaveAddr[IN] Device slave address
regAddr[IN] Register offset address
regData[OUT] Register data pointer
Returns
BOARD_SOK in case of success or appropriate error code.
void Board_fpdU960GetI2CAddr ( uint8_t *  chNum,
uint8_t *  i2cAddr,
uint32_t  csiInst 
)

Get ub960 i2c address.

This function is used to get the I2C address and channel details of UB960 module.

Parameters
chNum[IN] buffer to hold i2c channel number
i2cAddr[IN] buffer to hold i2c address
csiInst[IN] CSIRX Instance See BOARD_csiInst for more details.
Returns
In case of wrong parameters, chNum and i2cAddr are sent back as '0'.
Board_STATUS Board_fpdUb960CfgPG ( void *  handle,
Board_FpdModuleObj fpdModParams,
uint32_t  pgType 
)

FPD ub960 pattern generation configurations.

This function is used for configuring the pattern generator for FPD UB960

Parameters
handle[IN] Low level driver handle
fpdModParams[IN] FPD module params
pgType[IN] Pattern Generation Type See DESUB960_patternType for details.
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_fpdUb960DesInit ( void *  handle,
Board_FpdModuleObj fpdModParams 
)

Initializes the FPD UB960 module.

This function is used to initialize the fpd ub960 module

Parameters
handle[IN] Low level driver handle
fpdModParams[IN] FPD module params ] *
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_fpdUb960DesInitFusionBoardTIDA1130 ( void *  handle,
Board_FpdModuleObj fpdModParams 
)

Initializes the FPD UB960 module for OV2775 sensor module.

This function is used to initialize the fpd ub960 module for OV2775 sensor

Parameters
handle[IN] Low level driver handle
fpdModParams[IN] FPD module params ] *
Returns
BOARD_SOK in case of success or appropriate error code.
Board_STATUS Board_fpdUb960Cfg ( void *  handle,
Board_FpdModuleObj fpdModParams,
Board_I2cRegProgObj ub960Cfg 
)

FPD ub960 configurations.

This function is used for configuring the FPD UB960 de-serializer

Parameters
handle[IN] Low level driver handle
fpdModParams[IN] FPD module params
ub960Cfg[IN] Configuration Info
Returns
BOARD_SOK in case of success or appropriate error code.