![]() |
PDK API Guide for AM65xx
|
Application Interfaces provided by DS90UB925 FPD-Link device library.
Functions | |
| Board_STATUS | Board_fpdUb925SetRGBGateDEModeCtrl (void *handle, Board_FpdModuleObj *fpdModParams, uint8_t cfgMode) |
| RGB gate data enable mode control. More... | |
| Board_STATUS | Board_fpdUb925SetI2SChBModeCtrl (void *handle, Board_FpdModuleObj *fpdModParams, uint8_t cfgMode) |
| I2S channel-B mode control. More... | |
| Board_STATUS | Board_fpdUb925SetI2SChBOverrideModeCtrl (void *handle, Board_FpdModuleObj *fpdModParams, uint8_t cfgMode) |
| I2S channel-B override mode control. More... | |
| Board_STATUS | Board_fpdUb925SetI2STransSelModeCtrl (void *handle, Board_FpdModuleObj *fpdModParams, uint8_t cfgMode) |
| I2S transport select mode control. More... | |
| Board_STATUS | Board_fpdUb925SetRGB18bitModeCtrl (void *handle, Board_FpdModuleObj *fpdModParams, uint8_t cfgMode) |
| RGB 18-bit mode control. More... | |
| Board_STATUS | Board_fpdUb925GetPCLKLockStatus (void *handle, Board_FpdModuleObj *fpdModParams, bool *pclkLockStatus) |
| Get PCLK lock status. More... | |
| Board_STATUS Board_fpdUb925SetRGBGateDEModeCtrl | ( | void * | handle, |
| Board_FpdModuleObj * | fpdModParams, | ||
| uint8_t | cfgMode | ||
| ) |
RGB gate data enable mode control.
This function is used for configuring the serializer RGB gate DE mode
| handle | [IN] Low level driver handle |
| fpdModParams | [IN] FPD module params |
| cfgMode | [IN] Config mode - Indicates Enable or Disable |
| Board_STATUS Board_fpdUb925SetI2SChBModeCtrl | ( | void * | handle, |
| Board_FpdModuleObj * | fpdModParams, | ||
| uint8_t | cfgMode | ||
| ) |
I2S channel-B mode control.
This function is used for configuring the serializer I2S channel-B mode
| handle | [IN] Low level driver handle |
| fpdModParams | [IN] FPD module params |
| cfgMode | [IN] Config mode - Indicates Enable or Disable |
| Board_STATUS Board_fpdUb925SetI2SChBOverrideModeCtrl | ( | void * | handle, |
| Board_FpdModuleObj * | fpdModParams, | ||
| uint8_t | cfgMode | ||
| ) |
I2S channel-B override mode control.
This function is used for configuring the serializer I2S channel-B override mode
| handle | [IN] Low level driver handle |
| fpdModParams | [IN] FPD module params |
| cfgMode | [IN] Config mode - Indicates Enable or Disable |
| Board_STATUS Board_fpdUb925SetI2STransSelModeCtrl | ( | void * | handle, |
| Board_FpdModuleObj * | fpdModParams, | ||
| uint8_t | cfgMode | ||
| ) |
I2S transport select mode control.
This function is used for configuring the serializer I2S transport select mode
| handle | [IN] Low level driver handle |
| fpdModParams | [IN] FPD module params |
| cfgMode | [IN] Config mode - Indicates Enable or Disable |
| Board_STATUS Board_fpdUb925SetRGB18bitModeCtrl | ( | void * | handle, |
| Board_FpdModuleObj * | fpdModParams, | ||
| uint8_t | cfgMode | ||
| ) |
RGB 18-bit mode control.
This function is used for configuring the serializer RGB 18-bit mode
| handle | [IN] Low level driver handle |
| fpdModParams | [IN] FPD module params |
| cfgMode | [IN] Config mode - Indicates Enable or Disable |
| Board_STATUS Board_fpdUb925GetPCLKLockStatus | ( | void * | handle, |
| Board_FpdModuleObj * | fpdModParams, | ||
| bool * | pclkLockStatus | ||
| ) |
Get PCLK lock status.
This function is used for reading the serializer PCLK lock status
| handle | [IN] Low level driver handle |
| fpdModParams | [IN] FPD module parameters |
| pclkLockStatus | [IN/OUT] Buffer to hold PLL lock status |