The GIO Manager offers both the issue/reclaim model and the read/write
model to send and receive data from drivers that implement the IOM
interface as provided in ti/sysbios/io/iom.h.
The client can issue many buffers before reclaiming them.
Buffers are always reclaimed in the order that they were issued.
The client can optionally pass a user argument to issue(). This argument
can be retrieved with reclaim().
| const GIO_INOUT |
 |
mode for input & output
#define GIO_INOUT (UInt)0x3
| const GIO_INPUT |
 |
mode for input
#define GIO_INPUT (UInt)0x1
| const GIO_OUTPUT |
 |
mode for output
#define GIO_OUTPUT (UInt)0x2
| enum GIO_Model |
 |
model for IO channel
typedef enum GIO_Model {
GIO_Model_STANDARD,
// used for read, write, submit
GIO_Model_ISSUERECLAIM
// used for issue, reclaim, prime
} GIO_Model;
| typedef GIO_InitFxn |
 |
Init function type definition
typedef Void (*GIO_InitFxn)();
| typedef GIO_TappCallBack |
 |
application callback function used with GIO_submit()
typedef Void (*GIO_TappCallBack)(Ptr,Int,Ptr,SizeT);
| struct GIO_AppCallback |
 |
Application Callback Structure
typedef struct GIO_AppCallback {
Ptr arg;
} GIO_AppCallback;
DETAILS
Used with GIO_submit() for asynchronous callback.
| config GIO_A_badModel // module-wide |
 |
Asserted in GIO_read(), GIO_write() if I/O model is not
STANDARD or in GIO_issue(), GIO_reclaim(), or GIO_prime() if the
I/O model is not ISSUERECLAIM
| config GIO_E_createFailed // module-wide |
 |
Error raised when driver's mdCreateChan() call fails
extern const Error_Id GIO_E_createFailed;
| config GIO_E_notFound // module-wide |
 |
Error raised when name not found in DeviceTable
| config GIO_deviceTableSize // module-wide |
 |
This configuration parameter has been deprecated. Use DEV.tableSize
extern const Int GIO_deviceTableSize;
| GIO_addDevice() // module-wide |
 |
This API has been deprecated. Use DEV_create()
Int GIO_addDevice(
String name,
Ptr fxns,
GIO_InitFxn initFxn,
Int devid,
Ptr params);
| GIO_removeDevice() // module-wide |
 |
This API has been deprecated. Use DEV_match() and DEV_delete()
Int GIO_removeDevice(String name);
| Module-Wide Built-Ins |
 |
// Get this module's unique id
Bool GIO_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool GIO_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 GIO_Module_getMask();
// Returns the diagnostics mask for this module
Void GIO_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
| Instance Object Types |
 |
typedef struct GIO_Object GIO_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct GIO_Struct GIO_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
| Instance Config Parameters |
 |
typedef struct GIO_Params {
// Instance config-params structure
// Common per-instance configs
Ptr chanParams;
// channel parameters
// I/O model
Int numPackets;
// Number of packets to use for asynchronous I/O
Ptr packets;
// The address of the buffer used for IOM packets
// ISync handle used to signal IO completion
UInt timeout;
// For blocking calls. Default is BIOS_WAIT_FOREVER
} GIO_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
| config GIO_Params.chanParams // instance |
 |
channel parameters
DETAILS
The chanParams parameter is a pointer that may be used to pass device
or domain-specific arguments to the mini-driver. The contents at the
specified address are interpreted by the mini-driver in a
device-specific manner.
| config GIO_Params.model // instance |
 |
I/O model
DETAILS
Set the model to STANDARD to use read(), write() and submit() APIs.
Set the model to ISSUERECLAIM to use issue(), reclaim(), and
prime() APIs.
The default for this parameter is STANDARD.
| config GIO_Params.numPackets // instance |
 |
Number of packets to use for asynchronous I/O
| config GIO_Params.packets // instance |
 |
The address of the buffer used for IOM packets
DETAILS
If set to 'null', the packets will be allocated from the heap
during runtime, otherwise the user may set this to a buffer of their
creation to be used for the IOM packets.
The packets will be split into
ti.sysbios.io.GIO.numPackets each the size of IOM_Packet.
Please note that if the packets is user supplied, then it is the user's
responsibility to ensure that it is aligned properly and is also large
enough to contain
ti.sysbios.io.GIO.numPackets number of
IOM_Packet packets. The size of packets buffer, if provided,
should be
sizeof(IOM_Packet) * numPackets
Example:
#define NUMPACKETS 2
IOM_Packet inPackets[NUMPACKETS];
GIO_Params params;
GIO_Params_init(¶ms);
params.numPackets = NUMPACKETS;
params.packets = inPackets;
| config GIO_Params.sync // instance |
 |
ISync handle used to signal IO completion
| config GIO_Params.timeout // instance |
 |
For blocking calls. Default is BIOS_WAIT_FOREVER
| Runtime Instance Creation |
 |
// Allocate and initialize a new instance object and return its handle
// Initialize a new instance object inside the provided structure
ARGUMENTS
name
name that identifies the IO stack
mode
mode of channel
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
An application calls GIO_create to create a GIO_Obj object and open
a communication channel. This function initializes the I/O channel
and opens the lower-level device driver channel. The GIO_create call
also creates the synchronization objects it uses and stores them in
the GIO_Obj object.
The name argument is the name specified for the device when it was
created in the configuration or at runtime.
The mode argument specifies the mode in which the device is to be
opened. This may be IOM_INPUT, IOM_OUTPUT, or IOM_INOUT.
If the status returned by the device is non-NULL, a status value is
placed at the address specified by the status parameter.
The GIO_create call allocates a list of IOM_Packet items as specified
by the numPackets member of the params structure and stores them in
the GIO_Obj object it creates.
| Instance Deletion |
 |
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
// Finalize the instance object inside the provided structure
| GIO_abort() // instance |
 |
Abort all pending IO
ARGUMENTS
handle
handle of a previously-created GIO instance object
RETURNS
IOM_COMPLETED on success, < 0 on failure
DETAILS
An application calls GIO_abort to abort all input and output from
the device. When this call is made, all pending calls are completed
with a status of GIO_ABORTED. An application uses this call to
return the device to its initial state. Usually this is done in
response to an unrecoverable error at the device level.
GIO_abort returns IOM_COMPLETED upon successfully aborting all
input and output requests. If an error occurs, the device returns a
negative value. The list of error values are defined in the
ti/sysbios/io/iom.h file.
A call to GIO_abort results in a call to the mdSubmit function of the
associated mini-driver. The IOM_ABORT command is passed to the
mdSubmit function. The mdSubmit call is typically a blocking call, so
calling GIO_abort can result in the thread blocking.
If using ISSUERECLAIM IO model, the the underlying device
connected to stream is idled as a result of calling abort and
all buffers are ready for reclaim(). The client needs to call
reclaim to get back the buffers. However the client will
NOT block when calling reclaim() after an abort().
| GIO_control() // instance |
 |
Send a control command to the driver
Int GIO_control(
GIO_Handle handle,
UInt cmd,
Ptr args);
ARGUMENTS
handle
handle of a previously-created GIO instance object
cmd
device specific command
args
pointer to device-specific arguments
RETURNS
IOM_COMPLETED on success, < 0 on failure
DETAILS
An application calls GIO_control to configure or perform control
functionality on the communication channel.
The cmd parameter may be one of the command code constants listed in
ti/sysbios/io/iom.h. A mini-driver may add command codes for
additional functionality.
The args parameter points to a data structure defined by the device to
allow control information to be passed between the device and the
application. This structure can be generic across a domain or
specific to a mini-driver. In some cases, this argument may point
directly to a buffer holding control data. In other cases, there
may be a level of indirection if the mini-driver expects a data
structure to package many components of data required for the control
operation. In the simple case where no data is required, this
parameter may just be a predefined command value.
GIO_control returns IOM_COMPLETED upon success. If an error occurs,
the device returns a negative value. For a list of error values, see
ti/sysbios/io/iom.h. A call to GIO_control results in a call to
the mdControl function of the associated mini-driver. The mdControl
call is typically a blocking call, so calling GIO_control can result
in blocking.
| GIO_flush() // instance |
 |
Drain output buffers and discard any pending input
ARGUMENTS
handle
handle of a previously-created GIO instance object
RETURNS
IOM_COMPLETED on success, < 0 on failure
DETAILS
An application calls GIO_flush to flush the input and output
channels of the device. All input data is discarded; all pending
output requests are completed. When this call is made, all pending
input calls are completed with a status of IOM_FLUSHED, and all
output calls are completed routinely.
This call returns IOM_COMPLETED upon successfully flushing all
input and output. If an error occurs, the device returns a negative
value. For a list of error values, see ti/sysbios/io/iom.h.
A call to GIO_flush results in a call to the mdSubmit function of
the associated mini-driver. The IOM_FLUSH command is passed to the
mdSubmit function. The mdSubmit call is typically a blocking call,
so calling GIO_flush can result in the thread blocking while waiting
for output calls to be completed.
| GIO_issue() // instance |
 |
Issue a buffer to the stream
Int GIO_issue(
GIO_Handle handle,
Ptr buf,
SizeT size,
UArg arg);
ARGUMENTS
handle
handle of a previously-created GIO instance object
buf
buffer pointer
size
size of buffer
arg
application arg
RETURNS
IOM_COMPLETED on success, < 0 on failure
DETAILS
This function issues a buffer to the stream for IO. This API is
non-blocking.
Failure of issue() indicates that the stream was not able to accept the
buffer being issued or that there was a error from the underlying
driver. Note that the error could be driver specific.
If issue() fails because of an underlying driver problem
abort should be called before attempting more I/O through the
stream.
The interpretation of the logical size of a buffer, is direction
dependent. For a stream opened in OUTPUT mode, the logical size
of the buffer indicates the number of minimum addressable units of of
data it contains.
For a stream opened in INPUT mode, the logical size
of a buffer indicates the number of minimum addressable units being
requested by the client. In either case, the logical size of the buffer
must be less than or equal to the physical size of the buffer.
issue() is used in conjunction with
reclaim. The issue() call
sends a buffer to a stream, and reclaim() retrieves a buffer
from a stream. In normal operation each issue() call is followed by an
reclaim() call.
Short bursts of multiple issue() calls can be made without an
intervening reclaim() call followed by short bursts of reclaim() calls,
but over the life of the stream issue() and reclaim() must be called
the same number of times. The number of issue() calls can exceed the
number of reclaim() calls by
maxIssues.
The client argument is not interpreted by IO or the underlying
modules, but is offered as a service to the stream client. All compliant
device drivers preserve the value of arg and maintain its association
with the data that it was issued with. arg provides a method for a
client to associate additional information with a particular buffer of
data. The arg is returned during reclaim().
| GIO_prime() // instance |
 |
Prime an OUTPUT stream instance
Int GIO_prime(
GIO_Handle handle,
Ptr buf,
SizeT size,
UArg arg);
ARGUMENTS
handle
handle of a previously-created GIO instance object
buf
buffer pointer
size
size of buffer
arg
app arg
RETURNS
IOM_COMPLETED on success, < 0 on failure
DETAILS
This API facilitates buffering of an output channel. Consider a
task that constantly gets data from input channel and sends to an
output channel. To start with it may want to issue buffers to the
input channel and output channel to enable double buffering.
For an input channel there is no problem. For an output channel however
the buffer data is sent out through the peripheral and in the case of a
heterogenous system, the data will be sent to the other processor.
In such cases where the driver cannot handle dummy buffers,
IO_prime can be used to make buffers available instantly for
reclaim without actually sending the buffers to the driver.
This API is non-blocking.
The primary use of prime() is used when applications want to prime
an output channel at startup, without sending data to the driver.
This allows them to reclaim and issue in their task.
Failure of prime() indicates that the stream was not able to accept the
buffer being issued due to un-avaibailibity of IO packets.
The client argument is not interpreted by IO.
| GIO_read() // instance |
 |
Synchronous read command
Int GIO_read(
GIO_Handle handle,
Ptr buf,
SizeT *
pSize);
ARGUMENTS
handle
handle of a previously-created GIO instance object
buf
buffer pointer
pSize
pointer to size of buffer (INPUT/OUTPUT parameter)
RETURNS
IOM_COMPLETED on success, < 0 on failure
DETAILS
An application calls GIO_read to read a specified number of MADUs
(minimum addressable data units) from the communication channel.
The buf parameter points to a device-defined data structure for
passing buffer data between the device and the application. This
structure may be generic across a domain or specific to a single
mini-driver. In some cases, this parameter may point directly to a
buffer that holds the read data. In other cases, this parameter may
point to a structure that packages buffer information, size, offset
to be read from, and other device-dependent data. For example, for
video capture devices this structure may contain pointers to RGB
buffers, their sizes, video format, and a host of data required for
reading a frame from a video capture device. Upon a successful read,
this argument points to the returned data.
The pSize parameter points to the size of the buffer or data
structure pointed to by the buf parameter. When the function
returns, this parameter points to the number of MADUs read from the
device. This parameter is relevant only if the buf parameter points
to a raw data buffer. In cases where it points to a device-defined
structure it is redundant -- the size of the structure is known to
the mini-driver and the application. At most, it can be used for
error checking.
GIO_read returns IOM_COMPLETED upon successfully reading the
requested number of MADUs from the device. If an error occurs,
the device returns a negative value. For a list of error values,
see ti/sybios/io/iom.h.
A call to GIO_read results in a call to the mdSubmit function of
the associated mini-driver. The IOM_READ command is passed to the
mdSubmit function. The mdSubmit call is typically a blocking call,
so calling GIO_read can result in the thread blocking.
| GIO_reclaim() // instance |
 |
Reclaim a buffer that was previously issued by calling issue
Int GIO_reclaim(
GIO_Handle handle,
Ptr *
pBuf,
SizeT *
pSize,
UArg *
pArg);
ARGUMENTS
handle
handle of a previously-created GIO instance object
pBuf
returned buffer pointer
pSize
pointer to size of buffer (OUTPUT parameter)
pArg
pointer to client arg. Can be null.
RETURNS
IOM_COMPLETED on success, < 0 on failure
DETAILS
reclaim() is used to request a buffer back from a stream.
If a stream was created in OUTPUT mode, then reclaim() returns a
processed buffer, and size is zero. If a stream was opened in
INPUT mode, reclaim() returns a full buffer, and size is the number
of minimum addressable units of data in the buffer.
reclaim() calls Sync_wait() with the timeout specified when the
channel was created. For the default SyncSem, reclaim() blocks
until a buffer can be returned to the caller, or until a timeout occurs.
Failure of reclaim() indicates that no buffer was returned to
the client. Therefore, if reclaim() fails, the client should
not attempt to de-reference pBuf, since it is not guaranteed to contain
a valid buffer pointer.
reclaim() is used in conjunction with
issue to operate
a stream. The issue() call sends a buffer to a stream, and
reclaim() retrieves a buffer from a stream. In normal operation
each issue call is followed by an reclaim call.
Short bursts of multiple issue() calls can be made without an
intervening reclaim() call followed by short bursts of reclaim() calls,
but over the life of the stream issue() and reclaim() must be called
the same number of times. The number of issue() calls can exceed the
number of reclaim() calls by
maxIssues.
A reclaim() call should not be made without at least one
outstanding issue() call. Calling reclaim() with no
outstanding issue() calls results in an error
E_noBuffersIssued
reclaim() only returns buffers that were passed in using issue(). It
also returns the buffers in the same order that they were issued.
reclaim() returns the size transferred in case of success.
It returns zero when an error is caught. In case of timeout, the error
is
E_timeout.
| GIO_submit() // instance |
 |
Submit an IO job to the mini-driver
ARGUMENTS
handle
handle of a previously-created GIO instance object
cmd
driver specific packet command
buf
buffer pointer
pSize
pointer to size of buffer (INPUT/OUTPUT parameter)
appCallBack
pointer to application callback structure
RETURNS
IOM_COMPLETED on success, < 0 on failure
DETAILS
GIO_submit is not typically called by applications. Instead, it is
used internally and for user-defined extensions to the GIO module.
The cmd parameter is IOM_READ, IOM_WRITE, IOM_ABORT or IOM_FLUSH
when used internally. A mini driver may add command codes for
additional functionality.
The bufp parameter points to a device-defined data structure for
passing buffer data between the device and the application. This
structure may be generic across a domain or specific to a single
mini-driver. In some cases, this parameter may point directly to
a buffer that holds the data. In other cases, this parameter may
point to a structure that packages buffer information, size, offset
to be read from, and other device-dependent data.
The pSize parameter points to the size of the buffer or data structure
pointed to by the bufp parameter. When the function returns, this
parameter points to the number of MADUs transferred to or from the
device. This parameter is relevant only if the bufp parameter points
to a raw data buffer. In cases where it points to a device-defined
structure it is redundant -- the size of the structure is known to
the mini-driver and the application. At most, it can be used for
error checking.
The appCallback parameter points to either a callback structure that
contains the callback function to be called when the request completes.
queued request is completed, the callback routine (if specified) is
invoked (i.e. blocking). If the appCallback parameter is NULL, then
the call to GIO_submit() will be synchronous and will not return
until IO is complete (or an error occurs).
GIO_submit returns IOM_COMPLETED upon successfully carrying out
the requested functionality. If the request is queued, then a status of
IOM_PENDING is returned. If an error occurs, the device returns a
negative value. For a list of error values, see ti/sysbios/io/iom.h.
A call to GIO_submit results in a call to the mdSubmit function of
the associated mini-driver. The specified command is passed to the
mdSubmit function.
| GIO_write() // instance |
 |
Synchronous write command
Int GIO_write(
GIO_Handle handle,
Ptr buf,
SizeT *
pSize);
ARGUMENTS
handle
handle of a previously-created GIO instance object
buf
buffer pointer
pSize
pointer to size of buffer (INPUT/OUTPUT parameter)
RETURNS
IOM_COMPLETED on success, < 0 on failure
DETAILS
An application calls GIO_write to write a specified number of MADUs
(minimum addressable data units) from the communication channel.
The buf parameter points to a device-defined data structure for
passing buffer data between the device and the application. This
structure may be generic across a domain or specific to a single
mini-driver. In some cases, this parameter may point directly to a
buffer that holds the write data. In other cases, this parameter may
point to a structure that packages buffer information, size, offset
to be write from, and other device-dependent data. For example, for
video capture devices this structure may contain pointers to RGB
buffers, their sizes, video format, and a host of data required for
reading a frame from a video capture device.
The pSize parameter points to the size of the buffer or data
structure pointed to by the buf parameter. When the function
returns, this parameter points to the number of MADUs written to the
device. This parameter is relevant only if the buf parameter points
to a raw data buffer. In cases where it points to a device-defined
structure it is redundant -- the size of the structure is known to
the mini-driver and the application. At most, it can be used for
error checking.
GIO_write returns IOM_COMPLETED upon successfully writing the
requested number of MADUs from the device. If an error occurs,
the device returns a negative value. For a list of error values,
see ti/sybios/io/iom.h.
A call to GIO_write results in a call to the mdSubmit function of
the associated mini-driver. The IOM_WRITE command is passed to the
mdSubmit function. The mdSubmit call is typically a blocking call,
so calling GIO_write can result in the thread blocking.
| Instance Built-Ins |
 |
Int GIO_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object
| const GIO.INOUT |
 |
mode for input & output
C SYNOPSIS
| const GIO.INPUT |
 |
mode for input
C SYNOPSIS
| const GIO.OUTPUT |
 |
mode for output
C SYNOPSIS
| enum GIO.Model |
 |
model for IO channel
values of type GIO.Model
const GIO.Model_STANDARD;
// used for read, write, submit
const GIO.Model_ISSUERECLAIM;
// used for issue, reclaim, prime
C SYNOPSIS
| struct GIO.AppCallback |
 |
Application Callback Structure
var obj = new GIO.AppCallback;
obj.fxn = Void(*)(Ptr,Int,Ptr,SizeT) ...
obj.arg = Ptr ...
DETAILS
Used with GIO_submit() for asynchronous callback.
C SYNOPSIS
| metaonly struct GIO.BasicView |
 |
var obj = new GIO.BasicView;
obj.label = String ...
obj.freeCount = UInt ...
obj.doneCount = UInt ...
obj.submitCount = UInt ...
obj.model = String ...
obj.mode = String ...
obj.userSuppliedSync = Bool ...
| config GIO.A_badModel // module-wide |
 |
Asserted in GIO_read(), GIO_write() if I/O model is not
STANDARD or in GIO_issue(), GIO_reclaim(), or GIO_prime() if the
I/O model is not ISSUERECLAIM
msg: "A_badModel: invalid use of API for current I/O model"
};
C SYNOPSIS
| config GIO.E_createFailed // module-wide |
 |
Error raised when driver's mdCreateChan() call fails
msg: "E_createFailed: mdCreateChan returned error %d"
};
C SYNOPSIS
| config GIO.E_notFound // module-wide |
 |
Error raised when name not found in DeviceTable
msg: "E_notFound: %s name not found"
};
C SYNOPSIS
| config GIO.deviceTableSize // module-wide |
 |
This configuration parameter has been deprecated. Use DEV.tableSize
GIO.deviceTableSize = Int 8;
C SYNOPSIS
| metaonly config GIO.common$ // module-wide |
 |
Common module configuration parameters
DETAILS
All modules have this configuration parameter. Its name contains the '$'
character to ensure it does not conflict with configuration parameters
declared by the module. This allows new configuration parameters to be
added in the future without any chance of breaking existing modules.
| metaonly config GIO.rovViewInfo // module-wide |
 |
| metaonly GIO.addDeviceMeta() // module-wide |
 |
This API has been deprecated. Use DEV.create()
GIO.addDeviceMeta(String name, String fxns, String initFxn, Int devid, String params) returns Void
| Instance Config Parameters |
 |
var params = new GIO.Params;
// Instance config-params object
params.chanParams = Ptr null;
// channel parameters
// I/O model
params.numPackets = Int 2;
// Number of packets to use for asynchronous I/O
params.packets = Ptr null;
// The address of the buffer used for IOM packets
// ISync handle used to signal IO completion
params.timeout = UInt ~(0);
// For blocking calls. Default is BIOS_WAIT_FOREVER
| config GIO.Params.chanParams // instance |
 |
channel parameters
var params = new GIO.Params;
...
params.chanParams = Ptr null;
DETAILS
The chanParams parameter is a pointer that may be used to pass device
or domain-specific arguments to the mini-driver. The contents at the
specified address are interpreted by the mini-driver in a
device-specific manner.
C SYNOPSIS
| config GIO.Params.model // instance |
 |
I/O model
var params = new GIO.Params;
...
DETAILS
Set the model to STANDARD to use read(), write() and submit() APIs.
Set the model to ISSUERECLAIM to use issue(), reclaim(), and
prime() APIs.
The default for this parameter is STANDARD.
C SYNOPSIS
| config GIO.Params.numPackets // instance |
 |
Number of packets to use for asynchronous I/O
var params = new GIO.Params;
...
params.numPackets = Int 2;
C SYNOPSIS
| config GIO.Params.packets // instance |
 |
The address of the buffer used for IOM packets
var params = new GIO.Params;
...
params.packets = Ptr null;
DETAILS
If set to 'null', the packets will be allocated from the heap
during runtime, otherwise the user may set this to a buffer of their
creation to be used for the IOM packets.
The packets will be split into
ti.sysbios.io.GIO.numPackets each the size of IOM_Packet.
Please note that if the packets is user supplied, then it is the user's
responsibility to ensure that it is aligned properly and is also large
enough to contain
ti.sysbios.io.GIO.numPackets number of
IOM_Packet packets. The size of packets buffer, if provided,
should be
sizeof(IOM_Packet) * numPackets
Example:
#define NUMPACKETS 2
IOM_Packet inPackets[NUMPACKETS];
GIO_Params params;
GIO_Params_init(¶ms);
params.numPackets = NUMPACKETS;
params.packets = inPackets;
C SYNOPSIS
| config GIO.Params.sync // instance |
 |
ISync handle used to signal IO completion
var params = new GIO.Params;
...
C SYNOPSIS
| config GIO.Params.timeout // instance |
 |
For blocking calls. Default is BIOS_WAIT_FOREVER
var params = new GIO.Params;
...
params.timeout = UInt ~(0);
C SYNOPSIS
| Static Instance Creation |
 |
// Allocate instance config-params
params.config = ...
// Assign individual configs
var inst = GIO.create(String name, UInt mode, params);
// Create an instance-object
ARGUMENTS
name
name that identifies the IO stack
mode
mode of channel
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
An application calls GIO_create to create a GIO_Obj object and open
a communication channel. This function initializes the I/O channel
and opens the lower-level device driver channel. The GIO_create call
also creates the synchronization objects it uses and stores them in
the GIO_Obj object.
The name argument is the name specified for the device when it was
created in the configuration or at runtime.
The mode argument specifies the mode in which the device is to be
opened. This may be IOM_INPUT, IOM_OUTPUT, or IOM_INOUT.
If the status returned by the device is non-NULL, a status value is
placed at the address specified by the status parameter.
The GIO_create call allocates a list of IOM_Packet items as specified
by the numPackets member of the params structure and stores them in
the GIO_Obj object it creates.