module ti.sysbios.heaps.HeapMultiBuf

Multiple fixed size buffer heap manager

The HeapMultiBuf manager provides functions to allocate and free storage from a heap of type HeapMultiBuf which inherits from IHeap. HeapMultiBuf manages multiple fixed-size memory buffers. Each buffer contains a fixed number of allocable memory 'blocks' of the same size. Simply put, a HeapMultiBuf instance manages a collection of HeapBuf instances. HeapMultiBuf is intended as a fast and deterministic memory manager which can service requests for blocks of arbitrary size. [ more ... ]
C synopsis target-domain sourced in ti/sysbios/heaps/HeapMultiBuf.xdc
#include <ti/sysbios/heaps/HeapMultiBuf.h>
Functions
Void
Void
Void
Void
Functions common to all IHeap modules
Ptr 
Void 
Void 
Bool 
Functions common to all target instances
Functions common to all target modules
Typedefs
typedef struct
typedef struct
typedef struct
Constants
extern const Assert_Id 
extern const Error_Id 
 
DETAILS
The HeapMultiBuf manager provides functions to allocate and free storage from a heap of type HeapMultiBuf which inherits from IHeap. HeapMultiBuf manages multiple fixed-size memory buffers. Each buffer contains a fixed number of allocable memory 'blocks' of the same size. Simply put, a HeapMultiBuf instance manages a collection of HeapBuf instances. HeapMultiBuf is intended as a fast and deterministic memory manager which can service requests for blocks of arbitrary size.
An example HeapMultiBuf instance might have sixteen 32-byte blocks in one buffer, and four 128-byte blocks in another buffer. A request for memory will be serviced by the smallest possible block, so a request for 100 bytes would receive a 128-byte block in our example.
Allocating from HeapMultiBuf will try to return a block from the first buffer which has:
1. A block size that is >= to the requested size
AND
2. An alignment that is >= to the requested alignment
If the first matching buffer is empty, HeapMultiBuf will only continue searching for a block if 'block borrowing' is enabled (see Block Borrowing).

HeapMultiBuf and HeapBuf

The HeapMultiBuf module is built on top of the HeapBuf module. Each buffer in a HeapMultiBuf is in fact managed by a HeapBuf instance. Configuration of a HeapMultiBuf is done by providing an array of configured HeapBuf parameter structures. Refer to the HeapBuf documentation for information on the buffer parameters. All of the documentation and parameters for HeapBuf apply equally to HeapMultiBuf. Another consequence of this is that configuration checking is left to the HeapBuf module. If a buffer in a HeapMultiBuf has been incorrectly configured (with blockSize = 0, for example), HeapBuf, not HeapMultiBuf, will raise an Assert. Since HeapMultiBuf is built on HeapBuf, it simply performs the logic to determine which HeapBuf to allocate a block from or which HeapBuf to free a block to.

Configuration Example

The following configuration code creates a HeapMultiBuf instance which manages 3 pools of 10 blocks each, with block sizes of 64, 128 and 256.
  var HeapMultiBuf = xdc.useModule('ti.sysbios.heaps.HeapMultiBuf');
  var HeapBuf = xdc.useModule('ti.sysbios.heaps.HeapBuf');

  // Create parameter structure for HeapMultiBuf instance.
  var hmbParams = new HeapMultiBuf.Params();
  hmbParams.numBufs = 3;

  // Create the parameter structures for each of the three
  // HeapBufs to be managed by the HeapMultiBuf instance.
  hmbParams.bufParams.$add(new HeapBuf.Params());
  hmbParams.bufParams[0].blockSize = 64;
  hmbParams.bufParams[0].numBlocks = 10;

  hmbParams.bufParams.$add(new HeapBuf.Params());
  hmbParams.bufParams[1].blockSize = 128;
  hmbParams.bufParams[1].numBlocks = 10;

  hmbParams.bufParams.$add(new HeapBuf.Params());
  hmbParams.bufParams[2].blockSize = 256;
  hmbParams.bufParams[2].numBlocks = 10;


  // Create the HeapMultiBuf instance, and assign the global handle
  // 'multiBufHeap' to it. Add '#include <xdc/cfg/global.h>' to your
  // .c file to reference the instance by this handle.
  Program.global.multiBufHeap = HeapMultiBuf.create(hmbParams);

Block Borrowing

HeapMultiBuf can support "block borrowing". With this feature turned on, if a request is made for a 32-byte block and none are available, HeapMultiBuf will continue looking for an available block in other buffers. When a borrowed block is freed, it will be returned back to its original buffer. Enabling Block Borrowing changes the determinism of alloc, since it may have to check any number of buffers to find an available block. Block borrowing may also occur, even if it is disabled, if a block of a particular size is requested with an alignment that is greater than the configured alignment for that block size. For example, a HeapMultiBuf is configured with a buffer of 32-byte blocks with an alignment of 8, and a buffer of 64-byte blocks with an alignment of 16. If a request is made for a 32-byte block with an alignment of 16, it will be serviced by the buffer of 64-byte blocks.

Static vs. Dynamic Creation

As with HeapBuf, a statically created HeapMultiBuf instance will ignore the bufSize and buf parameters. Dynamic creates require all of the parameters. It should be noted that static creates are ideal if code space is a concern; dynamically creating a HeapMultiBuf requires a relatively large amount of initialization code to be pulled in to the executable.

Block Sizes and Alignment

  • A buffer with a requested alignment of 0 will receive the target- specific minimum alignment.
  • The actual block sizes will be a multiple of the alignment. For example, if a buffer is configured to have 56-byte blocks with an alignment of 32, HeapMultiBuf will actually create 64-byte blocks. When providing the buffer for a dynamic create, make sure it is large enough to take this into account.
  • Multiple buffers with the same block size ARE allowed. This may occur, for example, if sizeof is used to specify the block sizes.
  • If any buffers have both the same block size and alignment, they will be merged. If this is a problem, consider managing these buffers directly with HeapBuf objects.

Real-Time Concerns

Allocation from and freeing to a HeapMultiBuf instance is non-blocking. HeapMultiBuf is deterministic:
  • A call to alloc will always take the same amount of time for a given block size (with block borrowing disabled).
  • The worst case call to free is constant and proportional to the number of buffers managed.

Restrictions

  • Align parameters must be a power of 2.
  • The buffers passed to dynamically create a HeapMultiBuf must be aligned according to the alignment parameter, and must be large enough to account for the actual block size after it has been rounded up to a multiple of the alignment.
  • Buffers must be provided to dynamically create a HeapMultiBuf, and cannot be provided to statically create a HeapMultiBuf.

Unconstrained Functions

All functions

Calling Context

Function Hwi Swi Task Main Startup
Params_init Y Y Y Y Y
alloc Y Y Y Y N
construct N* N* Y Y N
create N* N* Y Y N
delete N* N* Y Y N
destruct N* N* Y Y N
free Y Y Y Y N
getStats Y Y Y Y N
isBlocking Y Y Y Y N
Definitions:
  • Hwi: API is callable from a Hwi thread.
  • Swi: API is callable from a Swi thread.
  • Task: API is callable from a Task thread.
  • Main: API is callable during any of these phases:
    • In your module startup after this module is started (e.g. HeapMultiBuf_Module_startupDone() returns TRUE).
    • During xdc.runtime.Startup.lastFxns.
    • During main().
    • During BIOS.startupFxns.
  • Startup: API is callable during any of these phases:
    • During xdc.runtime.Startup.firstFxns.
    • In your module startup before this module is started (e.g. HeapMultiBuf_Module_startupDone() returns FALSE).
  • *: Assuming blocking Heap is used for creation.
  • **: Assuming GateMutex is used as HeapMem's Gate.
  • + : Cannot use HeapMem object while it is being restored.
 
config HeapMultiBuf_A_blockNotFreed  // module-wide

Invalid block pointer

C synopsis target-domain
extern const Assert_Id HeapMultiBuf_A_blockNotFreed;
 
DETAILS
This Assert is raised if a call to free does not successfully free the block back to any of the buffers. Indicates that the block pointer is invalid, or that the HeapMultiBuf state has been corrupted.
 
config HeapMultiBuf_E_size  // module-wide

Raised when requested size exceeds all blockSizes

C synopsis target-domain
extern const Error_Id HeapMultiBuf_E_size;
 
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId HeapMultiBuf_Module_id();
// Get this module's unique id
 
Bool HeapMultiBuf_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle HeapMultiBuf_Module_heap();
// The heap from which this module allocates memory
 
Bool HeapMultiBuf_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 HeapMultiBuf_Module_getMask();
// Returns the diagnostics mask for this module
 
Void HeapMultiBuf_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types

C synopsis target-domain
typedef struct HeapMultiBuf_Object HeapMultiBuf_Object;
// Opaque internal representation of an instance object
 
typedef HeapMultiBuf_Object *HeapMultiBuf_Handle;
// Client reference to an instance object
 
typedef struct HeapMultiBuf_Struct HeapMultiBuf_Struct;
// Opaque client structure large enough to hold an instance object
 
HeapMultiBuf_Handle HeapMultiBuf_handle(HeapMultiBuf_Struct *structP);
// Convert this instance structure pointer into an instance handle
 
HeapMultiBuf_Struct *HeapMultiBuf_struct(HeapMultiBuf_Handle handle);
// Convert this instance handle into an instance structure pointer
Instance Config Parameters

C synopsis target-domain
typedef struct HeapMultiBuf_Params {
// Instance config-params structure
    IInstance_Params *instance;
    // Common per-instance configs
    Bool blockBorrow;
    // Turn block borrowing on (true) or off (false)
    HeapBuf_Params bufParams[];
    // Config parameters for each buffer
    Int numBufs;
    // Number of memory buffers
} HeapMultiBuf_Params;
 
Void HeapMultiBuf_Params_init(HeapMultiBuf_Params *params);
// Initialize this config-params structure with supplier-specified defaults before instance creation
 
config HeapMultiBuf_Params.blockBorrow  // instance

Turn block borrowing on (true) or off (false)

C synopsis target-domain
      ...
    Bool blockBorrow;
 
DETAILS
With block borrowing on, if there are no blocks available of the requested size, then alloc will look for a larger block to return. Calls to alloc which borrow blocks will be slower, and will cause internal fragmentation of the heap (until the block is freed), so it is ideal to configure a HeapMultiBuf such that block borrowing is not needed.
 
config HeapMultiBuf_Params.bufParams  // instance

Config parameters for each buffer

C synopsis target-domain
      ...
    HeapBuf_Params bufParams[];
 
DETAILS
Each buffer in a HeapMultiBuf is in fact managed by a HeapBuf instance. Configuration of a HeapMultiBuf is done by providing an array of configured HeapBuf parameter structures. Refer to the HeapBuf documentation for information on the buffer parameters. All of the documentation and parameters for HeapBuf apply to HeapMultiBuf. If a buffer is configured incorrectly, HeapBuf, not HeapMultiBuf, will raise an Assert.
 
config HeapMultiBuf_Params.numBufs  // instance

Number of memory buffers

C synopsis target-domain
      ...
    Int numBufs;
 
DETAILS
The number of different fixed size memory buffers that are managed by the heap instance. The bufParams array has length numBufs.
The default number of buffers is 0.
Runtime Instance Creation

C synopsis target-domain
HeapMultiBuf_Handle HeapMultiBuf_create(const HeapMultiBuf_Params *params, Error_Block *eb);
// Allocate and initialize a new instance object and return its handle
 
Void HeapMultiBuf_construct(HeapMultiBuf_Struct *structP, const HeapMultiBuf_Params *params, Error_Block *eb);
// Initialize a new instance object inside the provided structure
ARGUMENTS
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
See specific IHeap implementation for parameters used.
Instance Deletion

C synopsis target-domain
Void HeapMultiBuf_delete(HeapMultiBuf_Handle *handleP);
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
 
Void HeapMultiBuf_destruct(HeapMultiBuf_Struct *structP);
// Finalize the instance object inside the provided structure
 
HeapMultiBuf_alloc()  // instance

Allocates a block of memory from the heap

C synopsis target-domain
Ptr HeapMultiBuf_alloc(HeapMultiBuf_Handle handle, SizeT size, SizeT align, Error_Block *eb);
 
ARGUMENTS
handle — handle of a previously-created HeapMultiBuf instance object
size — size (in MADUs) of the block
align — alignment (in MADUs) of the block
eb — pointer to error block
DETAILS
This method returns a block of memory from the heap. It is called by the xdc.runtime.Memory.alloc() function.
HEAPMULTIBUF
HeapMultiBuf will return a block that is >= 'size' with an alignment that is >= 'align'. The HeapMultiBuf will attempt to service a request for any size; the specified size does not need to match the configured block sizes of the buffers.
RETURNS
Returns the address of the allocated memory.
 
HeapMultiBuf_free()  // instance

Free a block of memory back to the heap

C synopsis target-domain
Void HeapMultiBuf_free(HeapMultiBuf_Handle handle, Ptr block, SizeT size);
 
ARGUMENTS
handle — handle of a previously-created HeapMultiBuf instance object
block — non-NULL address of allocated block to free
size — size (in MADUs) of the block of memory to free
DETAILS
This method gives back a block of memory to a heap. It is called by the xdc.runtime.Memory.free() function.
HEAPMULTIBUF
HeapMultiBuf ignores the 'size' parameter to free. It determines the correct buffer to free the block to by comparing addresses.
 
HeapMultiBuf_getStats()  // instance

Retrieve the statistics from the heap

C synopsis target-domain
Void HeapMultiBuf_getStats(HeapMultiBuf_Handle handle, Memory_Stats *stats);
 
ARGUMENTS
handle — handle of a previously-created HeapMultiBuf instance object
stats — non-NULL pointer to an output buffer
DETAILS
The caller passes in a pointer to a xdc.runtime.Memory.Stats structure and getStats fills in this structure.
This function is called by the xdc.runtime.Memory.getStats() function.
 
HeapMultiBuf_isBlocking()  // instance

Returns whether the heap may block during an alloc() or free()

C synopsis target-domain
Bool HeapMultiBuf_isBlocking(HeapMultiBuf_Handle handle);
 
ARGUMENTS
handle — handle of a previously-created HeapMultiBuf instance object
HEAPMULTIBUF
This function always returns FALSE since the alloc/free never block on a resource.
RETURNS
If the heap might block, TRUE is returned. If the heap does not block, FALSE is returned.
Instance Convertors

C synopsis target-domain
IHeap_Handle HeapMultiBuf_Handle_upCast(HeapMultiBuf_Handle handle);
// unconditionally move one level up the inheritance hierarchy
 
HeapMultiBuf_Handle HeapMultiBuf_Handle_downCast(IHeap_Handle handle);
// conditionally move one level down the inheritance hierarchy; NULL upon failure
Instance Built-Ins

C synopsis target-domain
Int HeapMultiBuf_Object_count();
// The number of statically-created instance objects
 
HeapMultiBuf_Handle HeapMultiBuf_Object_get(HeapMultiBuf_Object *array, Int i);
// The handle of the i-th statically-created instance object (array == NULL)
 
HeapMultiBuf_Handle HeapMultiBuf_Object_first();
// The handle of the first dynamically-created instance object, or NULL
 
HeapMultiBuf_Handle HeapMultiBuf_Object_next(HeapMultiBuf_Handle handle);
// The handle of the next dynamically-created instance object, or NULL
 
IHeap_Handle HeapMultiBuf_Object_heap();
// The heap used to allocate dynamically-created instance objects
 
Types_Label *HeapMultiBuf_Handle_label(HeapMultiBuf_Handle handle, Types_Label *buf);
// The label associated with this instance object
 
String HeapMultiBuf_Handle_name(HeapMultiBuf_Handle handle);
// The name of this instance object
 
Configuration settings sourced in ti/sysbios/heaps/HeapMultiBuf.xdc
var HeapMultiBuf = xdc.useModule('ti.sysbios.heaps.HeapMultiBuf');
module-wide config parameters
        msg: "Invalid block address on the free. Failed to free block back to heap."
    };
        msg: "requested size is too big: handle=0x%x, size=%u"
    };
 
per-instance config parameters
    var params = new HeapMultiBuf.Params// Instance config-params object;
        params.bufParams// Config parameters for each buffer = HeapBuf.Params[] undefined;
        params.numBufs// Number of memory buffers = Int 0;
per-instance creation
    var inst = HeapMultiBuf.create// Create an instance-object(params);
 
 
config HeapMultiBuf.A_blockNotFreed  // module-wide

Invalid block pointer

Configuration settings
HeapMultiBuf.A_blockNotFreed = Assert.Desc {
    msg: "Invalid block address on the free. Failed to free block back to heap."
};
 
DETAILS
This Assert is raised if a call to free does not successfully free the block back to any of the buffers. Indicates that the block pointer is invalid, or that the HeapMultiBuf state has been corrupted.
C SYNOPSIS
 
config HeapMultiBuf.E_size  // module-wide

Raised when requested size exceeds all blockSizes

Configuration settings
HeapMultiBuf.E_size = Error.Desc {
    msg: "requested size is too big: handle=0x%x, size=%u"
};
 
C SYNOPSIS
 
metaonly config HeapMultiBuf.common$  // module-wide

Common module configuration parameters

Configuration settings
HeapMultiBuf.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
Instance Config Parameters

Configuration settings
var params = new HeapMultiBuf.Params;
// Instance config-params object
    params.blockBorrow = Bool false;
    // Turn block borrowing on (true) or off (false)
    params.bufParams = HeapBuf.Params[] undefined;
    // Config parameters for each buffer
    params.numBufs = Int 0;
    // Number of memory buffers
 
config HeapMultiBuf.Params.blockBorrow  // instance

Turn block borrowing on (true) or off (false)

Configuration settings
var params = new HeapMultiBuf.Params;
  ...
params.blockBorrow = Bool false;
 
DETAILS
With block borrowing on, if there are no blocks available of the requested size, then alloc will look for a larger block to return. Calls to alloc which borrow blocks will be slower, and will cause internal fragmentation of the heap (until the block is freed), so it is ideal to configure a HeapMultiBuf such that block borrowing is not needed.
C SYNOPSIS
 
config HeapMultiBuf.Params.bufParams  // instance

Config parameters for each buffer

Configuration settings
var params = new HeapMultiBuf.Params;
  ...
params.bufParams = HeapBuf.Params[] undefined;
 
DETAILS
Each buffer in a HeapMultiBuf is in fact managed by a HeapBuf instance. Configuration of a HeapMultiBuf is done by providing an array of configured HeapBuf parameter structures. Refer to the HeapBuf documentation for information on the buffer parameters. All of the documentation and parameters for HeapBuf apply to HeapMultiBuf. If a buffer is configured incorrectly, HeapBuf, not HeapMultiBuf, will raise an Assert.
C SYNOPSIS
 
config HeapMultiBuf.Params.numBufs  // instance

Number of memory buffers

Configuration settings
var params = new HeapMultiBuf.Params;
  ...
params.numBufs = Int 0;
 
DETAILS
The number of different fixed size memory buffers that are managed by the heap instance. The bufParams array has length numBufs.
The default number of buffers is 0.
C SYNOPSIS
Static Instance Creation

Configuration settings
var params = new HeapMultiBuf.Params;
// Allocate instance config-params
params.config =   ...
// Assign individual configs
 
var inst = HeapMultiBuf.create(params);
// Create an instance-object
ARGUMENTS
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
See specific IHeap implementation for parameters used.
generated on Tue, 19 May 2020 22:40:36 GMT