module ti.sysbios.hal.SecondsCallback

A Seconds module that calls user-supplied callbacks

ISeconds implementation that uses user callback functions This module provides a implementation of the ISystemSupport interface that simply calls back the user defined functions to enable the System module's functionality. [ more ... ]
C synopsis target-domain sourced in ti/sysbios/hal/SecondsCallback.xdc
#include <ti/sysbios/hal/SecondsCallback.h>
Functions common to all ISeconds modules
UInt32 
UInt32 
Void 
UInt32 
Functions common to all target modules
Typedefs
typedef UInt32 
typedef UInt32 
typedef Void 
typedef UInt32 
typedef struct
Constants
extern const SecondsCallback_GetFxn 
extern const SecondsCallback_SetFxn 
 
DETAILS
ISeconds implementation that uses user callback functions This module provides a implementation of the ISystemSupport interface that simply calls back the user defined functions to enable the System module's functionality.
Configuration is as shown below.
  var SecondsCallback = xdc.useModule('xdc.runtime.SecondsCallback');
  SecondsCallback.getFxn = "&userGetSeconds";
  SecondsCallback.setFxn = "&userSetSeconds";
  SecondsCallback.getTimeFxn = "&userGetTime";
  SecondsCallback.setTimeFxn = "&userSetTime";

 
typedef SecondsCallback_GetFxn

'get' function signature

C synopsis target-domain
typedef UInt32 (*SecondsCallback_GetFxn)();
 
 
typedef SecondsCallback_GetTimeFxn

'getTime' function signature

C synopsis target-domain
typedef UInt32 (*SecondsCallback_GetTimeFxn)(SecondsCallback_Time*);
 
 
typedef SecondsCallback_SetFxn

'set' function signature

C synopsis target-domain
typedef Void (*SecondsCallback_SetFxn)(UInt32);
 
 
typedef SecondsCallback_SetTimeFxn

'set' function signature

C synopsis target-domain
typedef UInt32 (*SecondsCallback_SetTimeFxn)(SecondsCallback_Time*);
 
 
struct SecondsCallback_Time

Structure to hold a time value in seconds plus nanoseconds

C synopsis target-domain
typedef struct SecondsCallback_Time {
    UInt32 secsHi;
    // Upper 32 bits for 64-bit seconds
    UInt32 secs;
    // Seconds
    UInt32 nsecs;
    // Nanoseconds
} SecondsCallback_Time;
 
 
config SecondsCallback_getFxn  // module-wide

User supplied 'get' function

C synopsis target-domain
extern const SecondsCallback_GetFxn SecondsCallback_getFxn;
 
DETAILS
This function is called when the application calls Seconds.get() function.
By default, this function is configured with a default function that returns 0.
 
config SecondsCallback_getTimeFxn  // module-wide

User supplied 'getTime' function

C synopsis target-domain
extern const SecondsCallback_GetTimeFxn SecondsCallback_getTimeFxn;
 
DETAILS
This function is called when the application calls Seconds.getTime() function.
By default, this function is configured with a default function that returns 0.
 
config SecondsCallback_setFxn  // module-wide

User supplied 'set' function

C synopsis target-domain
extern const SecondsCallback_SetFxn SecondsCallback_setFxn;
 
DETAILS
This function is called when the application calls Seconds.set() function.
By default, this function is configured with a default function that does nothing.
 
config SecondsCallback_setTimeFxn  // module-wide

User supplied 'set' function

C synopsis target-domain
extern const SecondsCallback_SetTimeFxn SecondsCallback_setTimeFxn;
 
DETAILS
This function is called when the application calls Seconds.setTime() function.
By default, this function is configured with a default function that returns 0.
 
SecondsCallback_get()  // module-wide

Returns number of seconds since 1970 (the Unix epoch)

C synopsis target-domain
UInt32 SecondsCallback_get();
 
DETAILS
The user must call Seconds_set() before making any calls to Seconds_get(), otherwise the value returned by Seconds_get() will be meaningless.
 
SecondsCallback_getTime()  // module-wide

Fills in a Seconds_Time structure with seconds and nanoseconds elapsed since 1970 (the Unix epoch)

C synopsis target-domain
UInt32 SecondsCallback_getTime(ISeconds_Time *ts);
 
DETAILS
Seconds_set() must have been called before making any calls to Seconds_getTime(), otherwise the value returned by Seconds_getTime() will be meaningless.
 
SecondsCallback_set()  // module-wide

Update the real time clock with number of seconds since 1970

C synopsis target-domain
Void SecondsCallback_set(UInt32 seconds);
 
DETAILS
Note: This function is non-reentrant.
 
SecondsCallback_setTime()  // module-wide

Update the real time clock with the number of seconds and nanoseconds that have elapsed since 1970 (the Unix epoch). The Seconds_Time structure passed to setTime() contains the seconds and nanoseconds to set the real time clock to. This API can be called instead of Seconds_set(), if finer granularity of the time is required

C synopsis target-domain
UInt32 SecondsCallback_setTime(ISeconds_Time *ts);
 
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId SecondsCallback_Module_id();
// Get this module's unique id
 
Bool SecondsCallback_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle SecondsCallback_Module_heap();
// The heap from which this module allocates memory
 
Bool SecondsCallback_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 SecondsCallback_Module_getMask();
// Returns the diagnostics mask for this module
 
Void SecondsCallback_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
Configuration settings sourced in ti/sysbios/hal/SecondsCallback.xdc
var SecondsCallback = xdc.useModule('ti.sysbios.hal.SecondsCallback');
module-wide constants & types
        obj.secsHi// Upper 32 bits for 64-bit seconds = UInt32  ...
        obj.secs// Seconds = UInt32  ...
        obj.nsecs// Nanoseconds = UInt32  ...
module-wide config parameters
    SecondsCallback.getFxn// User supplied 'get' function = UInt32(*)() "&ti_sysbios_hal_SecondsCallback_defaultGet";
    SecondsCallback.getTimeFxn// User supplied 'getTime' function = UInt32(*)(SecondsCallback.Time*) "&ti_sysbios_hal_SecondsCallback_defaultGetTime";
    SecondsCallback.setFxn// User supplied 'set' function = Void(*)(UInt32) "&ti_sysbios_hal_SecondsCallback_defaultSet";
    SecondsCallback.setTimeFxn// User supplied 'set' function = UInt32(*)(SecondsCallback.Time*) "&ti_sysbios_hal_SecondsCallback_defaultSetTime";
 
 
 
struct SecondsCallback.Time

Structure to hold a time value in seconds plus nanoseconds

Configuration settings
var obj = new SecondsCallback.Time;
 
    obj.secsHi = UInt32  ...
    // Upper 32 bits for 64-bit seconds
    obj.secs = UInt32  ...
    // Seconds
    obj.nsecs = UInt32  ...
    // Nanoseconds
 
C SYNOPSIS
 
config SecondsCallback.getFxn  // module-wide

User supplied 'get' function

Configuration settings
SecondsCallback.getFxn = UInt32(*)() "&ti_sysbios_hal_SecondsCallback_defaultGet";
 
DETAILS
This function is called when the application calls Seconds.get() function.
By default, this function is configured with a default function that returns 0.
C SYNOPSIS
 
config SecondsCallback.getTimeFxn  // module-wide

User supplied 'getTime' function

Configuration settings
SecondsCallback.getTimeFxn = UInt32(*)(SecondsCallback.Time*) "&ti_sysbios_hal_SecondsCallback_defaultGetTime";
 
DETAILS
This function is called when the application calls Seconds.getTime() function.
By default, this function is configured with a default function that returns 0.
C SYNOPSIS
 
config SecondsCallback.setFxn  // module-wide

User supplied 'set' function

Configuration settings
SecondsCallback.setFxn = Void(*)(UInt32) "&ti_sysbios_hal_SecondsCallback_defaultSet";
 
DETAILS
This function is called when the application calls Seconds.set() function.
By default, this function is configured with a default function that does nothing.
C SYNOPSIS
 
config SecondsCallback.setTimeFxn  // module-wide

User supplied 'set' function

Configuration settings
SecondsCallback.setTimeFxn = UInt32(*)(SecondsCallback.Time*) "&ti_sysbios_hal_SecondsCallback_defaultSetTime";
 
DETAILS
This function is called when the application calls Seconds.setTime() function.
By default, this function is configured with a default function that returns 0.
C SYNOPSIS
 
metaonly config SecondsCallback.common$  // module-wide

Common module configuration parameters

Configuration settings
SecondsCallback.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
generated on Tue, 19 May 2020 22:40:30 GMT