module ti.sysbios.family.shared.vayu.TimerSupport

Vayu Timer Support

The Vayu Timer Support module works in conjunction with the DMTimer module to manage the usage of the DMTimers by the various Vayu cores. [ more ... ]
C synopsis target-domain sourced in ti/sysbios/family/shared/vayu/TimerSupport.xdc
DETAILS
The Vayu Timer Support module works in conjunction with the DMTimer module to manage the usage of the DMTimers by the various Vayu cores.
This module provides a timer available mask. The application can modify this available mask in the .cfg script to choose a different set of timers.
The default value of the timer availMask depends on the target the application is being built for. The defaults are shown below:
  For Vayu or DRA7XX devices:
   --------------------------------------------
  | Target       | Default availMask           |
   --------------------------------------------
  | A15          | 0x0202 (GPTimer 2 & 10)     |
  | DSP          | 0x0030 (GPTimer 5 & 6)      |
  | IPU(Dual-M4) | 0x050C (GPTimer 3,4,9 & 11) |
  | ARP32        | 0x00C0 (GPTimer 7 & 8)      |
   --------------------------------------------

  For TDA3XX devices:
   --------------------------------------------
  | Target       | Default availMask           |
   --------------------------------------------
  | DSP          | 0x0003 (GPTimer 1 & 2)      |
  | IPU(Dual-M4) | 0x000C (GPTimer 3 & 4)      |
  | ARP32        | 0x00C0 (GPTimer 7 & 8)      |
   --------------------------------------------
NOTE
If the availMask is changed, the interrupt sources corresponding to the new Timer Ids may need to be mapped in the interrupt crossbar module if they are not mapped by default.
See Timer Mapping Tables to determine the default interruptNumber/eventId assigned to each DM Timer. In the Timer Mapping Table, an interrupt number of -1 implies the timer's interrupt source is not connected to the target cpu's interrupt controller. If you need to use a timer with an interrupt number of -1, you will need to first select an unused interrupt to use for the timer and then map the timer's interrupt source to the target cpu's interrupt controller using the Interrupt Crossbar module.
Below is an example showing how to statically override the default timer available mask in a configuration script for the DSP:
  var Timer = xdc.useModule('ti.sysbios.timers.dmtimer.Timer');
  var IntXbar = xdc.useModule('ti.sysbios.family.shared.vayu.IntXbar');
  var TimerSupport = xdc.useModule('ti.sysbios.family.shared.vayu.TimerSupport');

  // The new availability mask includes GP Timers 13, 14, 15 & 16.
  // The interrupt sources for these timers is not connected to the
  // DSP and need to be connected by the user.
  TimerSupport.availMask = 0xF000;

  // Connect GP Timer 13 to EventId 76 (XBAR Instance 45)
  IntXbar.connectMeta(45, 339);

  // Connect GP Timer 14 to EventId 77 (XBAR Instance 46)
  IntXbar.connectMeta(46, 340);

  // Connect GP Timer 15 to EventId 78 (XBAR Instance 47)
  IntXbar.connectMeta(47, 341);

  // Connect GP Timer 16 to EventId 81 (XBAR Instance 49)
  IntXbar.connectMeta(49, 342);

  // The DMTimer's timer mapping table shows that the intNum
  // for GP Timer 13, 14, 15 & 16 is -1 implying the intNum
  // has not been assigned by default. The below code utilizes
  // the DMTimer module's timerSettings array to assign
  // a default intNum to each of these timers.
  Timer.timerSettings[12].intNum = 14;
  Timer.timerSettings[13].intNum = 15;
  Timer.timerSettings[14].intNum = 4;
  Timer.timerSettings[15].intNum = 5;

  var TimerParams = new Timer.Params();
  TimerParams.period = 5000;
  TimerParams.runMode = Timer.RunMode_ONESHOT;
  TimerParams.periodType = Timer.PeriodType_MICROSECS;

  TimerParams.arg = 1;
  Timer.create(Timer.ANY, '&myIsr1', TimerParams);

  TimerParams.arg = 2;
  Timer.create(Timer.ANY, '&myIsr2', TimerParams);
Below is an example showing how to statically override the default timer available mask in a configuration script for the A15:
  var Timer = xdc.useModule('ti.sysbios.hal.Timer');
  var DMTimer = xdc.useModule('ti.sysbios.timers.dmtimer.Timer');

  // Override the default hal timer proxy for the A15 target
  Timer.TimerProxy = DMTimer;

  var TimerSupport = xdc.module('ti.sysbios.family.shared.vayu.TimerSupport');
  TimerSupport.availMask = 0x000F;

  var TimerParams = new Timer.Params();
  TimerParams.arg = 1;
  TimerParams.period = 5000;
  TimerParams.runMode = Timer.RunMode_ONESHOT;
  TimerParams.periodType = Timer.PeriodType_MICROSECS;

  Timer.create(Timer.ANY, '&myIsr', TimerParams);
 
config TimerSupport_availMask  // module-wide

Default available mask for dmtimers

C synopsis target-domain
extern const Bits32 TimerSupport_availMask;
 
DETAILS
Used to set Timer module's availMask. The default value of the timer availMask depends on the target the application is being built for. The defaults are shown below:
  For Vayu or DRA7XX devices:
   --------------------------------------------
  | Target       | Default availMask           |
   --------------------------------------------
  | A15          | 0x0202 (GPTimer 2 & 10)     |
  | DSP          | 0x0030 (GPTimer 5 & 6)      |
  | IPU(Dual-M4) | 0x050C (GPTimer 3,4,9 & 11) |
   --------------------------------------------

  For TDA3XX devices:
   --------------------------------------------
  | Target       | Default availMask           |
   --------------------------------------------
  | DSP          | 0x0003 (GPTimer 1 & 2)      |
  | IPU(Dual-M4) | 0x050C (GPTimer 3 & 3)      |
   --------------------------------------------
 
TimerSupport_enable()  // module-wide
C synopsis target-domain
Void TimerSupport_enable(UInt timerId, Error_Block *eb);
 
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId TimerSupport_Module_id();
// Get this module's unique id
 
Bool TimerSupport_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle TimerSupport_Module_heap();
// The heap from which this module allocates memory
 
Bool TimerSupport_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 TimerSupport_Module_getMask();
// Returns the diagnostics mask for this module
 
Void TimerSupport_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
Configuration settings sourced in ti/sysbios/family/shared/vayu/TimerSupport.xdc
var TimerSupport = xdc.useModule('ti.sysbios.family.shared.vayu.TimerSupport');
module-wide config parameters
 
 
 
config TimerSupport.availMask  // module-wide

Default available mask for dmtimers

Configuration settings
TimerSupport.availMask = Bits32 0x0;
 
DETAILS
Used to set Timer module's availMask. The default value of the timer availMask depends on the target the application is being built for. The defaults are shown below:
  For Vayu or DRA7XX devices:
   --------------------------------------------
  | Target       | Default availMask           |
   --------------------------------------------
  | A15          | 0x0202 (GPTimer 2 & 10)     |
  | DSP          | 0x0030 (GPTimer 5 & 6)      |
  | IPU(Dual-M4) | 0x050C (GPTimer 3,4,9 & 11) |
   --------------------------------------------

  For TDA3XX devices:
   --------------------------------------------
  | Target       | Default availMask           |
   --------------------------------------------
  | DSP          | 0x0003 (GPTimer 1 & 2)      |
  | IPU(Dual-M4) | 0x050C (GPTimer 3 & 3)      |
   --------------------------------------------
C SYNOPSIS
 
metaonly config TimerSupport.common$  // module-wide

Common module configuration parameters

Configuration settings
TimerSupport.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
generated on Tue, 19 May 2020 22:40:44 GMT