module ti.sysbios.family.shared.keystone3.SysUart

Implementation of xdc.runtime.ISystemSupport using ANSI C Standard Library

This implementation provides a fully functional implementation of all methods specified by ISystemSupport. As with all ISystemSupport modules, this module is the back-end for the xdc.runtime.System module. [ more ... ]
C synopsis target-domain sourced in ti/sysbios/family/shared/keystone3/SysUart.xdc
DETAILS
This implementation provides a fully functional implementation of all methods specified by ISystemSupport. As with all ISystemSupport modules, this module is the back-end for the xdc.runtime.System module.
This implementation relies on the target's runtime support libraries (i.e. fflush() and putchar()). Therefore the functions are re-entrant (thread-safe) if the underlying rts library is re-entrant.
 
enum SysUart_Uart

UART peripheral base address

C synopsis target-domain
typedef enum SysUart_Uart {
    SysUart_Uart0,
    // UART0 Base Address
    SysUart_Uart1,
    // UART1 Base Address
    SysUart_Uart2,
    // UART2 Base Address
    SysUart_Uart3,
    // UART3 Base Address
    SysUart_Uart4
    // UART4 Base Address
} SysUart_Uart;
 
DETAILS
These enumerations are the base addresses of the different UART peripherals.
 
config SysUart_uartBaseAddr  // module-wide
C synopsis target-domain
extern const Ptr SysUart_uartBaseAddr;
 
 
SysUart_abort()  // module-wide

Backend for xdc.runtime.System.abort()

C synopsis target-domain
Void SysUart_abort(CString str);
 
ARGUMENTS
str — message to output just prior to aborting
If non-NULL, this string should be output just prior to terminating.
DETAILS
This function is called by System.abort() prior to calling the ANSI C Standard library function abort(). So, to ensure the abort processing of the system's ANSI C Standard library completes, this function should return to its caller.
This abort function writes the string via putchar() and flushes via fflush() to stdout.
SEE
 
SysUart_exit()  // module-wide

Backend for xdc.runtime.System.exit()

C synopsis target-domain
Void SysUart_exit(Int stat);
 
ARGUMENTS
stat — status value passed to all "atexit" handlers
This value is passed to all "atexit" handles bound via System.atexit().
DETAILS
This function is called as part the normal "atexit" processing performed by the ANSI C Standard Library's exit() function; System.exit() directly calls ANSI exit().
This function is called after all "atexit" handlers bound via System.atexit() are run and it is always called while "inside" the the System gate.
To ensure that all exit processing of the system's ANSI C Standard Library completes, this function should return to its caller. Exit handlers bound using the ANSI C Standard Library atexit() function may run before or after this function.
This exit function flushes via fflush() to stdout.
SEE
 
SysUart_flush()  // module-wide

Backend for xdc.runtime.System.flush()

C synopsis target-domain
Void SysUart_flush();
 
DETAILS
This function is simply called by System_flush to output any characters buffered by the underlying SystemSupport module to an output device.
This flush function flushes via fflush() to stdout.
SEE
 
SysUart_putch()  // module-wide

Backend for xdc.runtime.System.printf() and xdc.runtime.System.putch()

C synopsis target-domain
Void SysUart_putch(Char ch);
 
ARGUMENTS
ch — character to output
DETAILS
Output a single character. This function is called by System_printf() to write each character of formated output specified by its arguments.
This function outputs the character via putchar().
SEE
 
SysUart_ready()  // module-wide

Test if character output can proceed

C synopsis target-domain
Bool SysUart_ready();
 
DETAILS
This function is called by System prior to performing any character output. If this function returns FALSE, the System functions that would normally call putch() simply return (with an appropriate error status) without ever calling putch.
This always returns TRUE.
SEE
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId SysUart_Module_id();
// Get this module's unique id
 
Bool SysUart_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle SysUart_Module_heap();
// The heap from which this module allocates memory
 
Bool SysUart_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 SysUart_Module_getMask();
// Returns the diagnostics mask for this module
 
Void SysUart_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
Configuration settings sourced in ti/sysbios/family/shared/keystone3/SysUart.xdc
var SysUart = xdc.useModule('ti.sysbios.family.shared.keystone3.SysUart');
module-wide constants & types
        const SysUart.Uart0// UART0 Base Address;
        const SysUart.Uart1// UART1 Base Address;
        const SysUart.Uart2// UART2 Base Address;
        const SysUart.Uart3// UART3 Base Address;
        const SysUart.Uart4// UART4 Base Address;
module-wide config parameters
    SysUart.uartBaseAddr//  = Ptr undefined;
 
 
 
enum SysUart.Uart

UART peripheral base address

Configuration settings
values of type SysUart.Uart
    const SysUart.Uart0;
    // UART0 Base Address
    const SysUart.Uart1;
    // UART1 Base Address
    const SysUart.Uart2;
    // UART2 Base Address
    const SysUart.Uart3;
    // UART3 Base Address
    const SysUart.Uart4;
    // UART4 Base Address
 
DETAILS
These enumerations are the base addresses of the different UART peripherals.
C SYNOPSIS
 
config SysUart.uartBaseAddr  // module-wide
Configuration settings
SysUart.uartBaseAddr = Ptr undefined;
 
C SYNOPSIS
 
metaonly config SysUart.common$  // module-wide

Common module configuration parameters

Configuration settings
SysUart.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
generated on Tue, 19 May 2020 22:40:43 GMT