module ti.sysbios.family.c7x.TaskSupport

C71 Task Support Module

C synopsis target-domain sourced in ti/sysbios/family/c7x/TaskSupport.xdc
 
config TaskSupport_defaultStackSize  // module-wide

Default Task stack size

C synopsis target-domain
extern const SizeT TaskSupport_defaultStackSize;
 
DETAILS
The C7x CPU uses 2 stacks during interrupt processing. The CPU automatically saves some context to the memory block to which the TCSP register points, and SW will save some context to the Task's SW stack during interrupt processing. In order to keep specification and processing compatible across different CPU targets, SYS/BIOS uses a single stack memory block for both of these stacks (although there isn't really any stacking with TCSP since there is a distinct block for each Task which is used only once). Due to HW alignment and size requirements for the TCSP block, there is a strict minimum of 16KB for the Task stack.
 
config TaskSupport_stackAlignment  // module-wide

Required stack alignment (in MAUs)

C synopsis target-domain
extern const UInt TaskSupport_stackAlignment;
 
DETAILS
The C7x CPU TCSP register requires this alignment (see defaultStackSize for further information).
 
config TaskSupport_A_stackSizeTooSmall  // module-wide

Asserted in TaskSupport_start

C synopsis target-domain
extern const Assert_Id TaskSupport_A_stackSizeTooSmall;
 
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId TaskSupport_Module_id();
// Get this module's unique id
 
Bool TaskSupport_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle TaskSupport_Module_heap();
// The heap from which this module allocates memory
 
Bool TaskSupport_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 TaskSupport_Module_getMask();
// Returns the diagnostics mask for this module
 
Void TaskSupport_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
Configuration settings sourced in ti/sysbios/family/c7x/TaskSupport.xdc
var TaskSupport = xdc.useModule('ti.sysbios.family.c7x.TaskSupport');
module-wide config parameters
 
        msg: "A_stackSizeTooSmall: Task stack size must be >= 16KB."
    };
 
 
 
config TaskSupport.defaultStackSize  // module-wide

Default Task stack size

Configuration settings
const TaskSupport.defaultStackSize = SizeT 0x4000;
 
DETAILS
The C7x CPU uses 2 stacks during interrupt processing. The CPU automatically saves some context to the memory block to which the TCSP register points, and SW will save some context to the Task's SW stack during interrupt processing. In order to keep specification and processing compatible across different CPU targets, SYS/BIOS uses a single stack memory block for both of these stacks (although there isn't really any stacking with TCSP since there is a distinct block for each Task which is used only once). Due to HW alignment and size requirements for the TCSP block, there is a strict minimum of 16KB for the Task stack.
C SYNOPSIS
 
config TaskSupport.stackAlignment  // module-wide

Required stack alignment (in MAUs)

Configuration settings
const TaskSupport.stackAlignment = UInt 0x2000;
 
DETAILS
The C7x CPU TCSP register requires this alignment (see defaultStackSize for further information).
C SYNOPSIS
 
config TaskSupport.A_stackSizeTooSmall  // module-wide

Asserted in TaskSupport_start

Configuration settings
TaskSupport.A_stackSizeTooSmall = Assert.Desc {
    msg: "A_stackSizeTooSmall: Task stack size must be >= 16KB."
};
 
C SYNOPSIS
 
metaonly config TaskSupport.common$  // module-wide

Common module configuration parameters

Configuration settings
TaskSupport.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
generated on Tue, 19 May 2020 22:40:42 GMT