|
|
|
TI-RTOS delivers components that enable engineers to develop applications on Texas Instruments micro-controller devices. The product is comprised of multiple software components and examples of how to use these components together. TI-RTOS gives developers a one-stop RTOS solution for developing applications for TI embedded microcontrollers. It provides an OS kernel, communications support, drivers, and more. It is tightly integrated with the Code Composer Studio development environment. In addition, examples are provided to demonstrate the use of each functional area and each supported device and as a starting point for your own projects.
The following documentation is available:
Click on the links below to view the release notes for the different products.
Examples are provided for the following boards:
To see what has changed in the TI-RTOS Drivers, see the separate TI-Drivers release notes in [as installed]/products/tidrivers_M_mm_pp_bb.
| Key | Summary |
|---|---|
| TIRTOS-100 | Restore tcp/udpSendReceive builds |
| TIRTOS-116 | Add examples to support the CC3200 WiFi to the TI-RTOS |
| TIRTOS-121 | Remove Concerto demo examples |
| TIRTOS-125 | Add macros or variables to help migration between different versions of TI-RTOS in IAR workbench |
| TIRTOS-127 | Add benchloop example to TI-RTOS |
| TIRTOS-133 | Example .c files should not include xdc/cfg/global.h |
| TIRTOS-140 | Console output in Linux doesn’t match in Windows for CC3200 tests |
| TIRTOS-146 | CC26xx/CC13xx kernel and instrumentation examples need to use the common .cfg |
| TIRTOS-148 | Doxygen for TIRTOS for TivaC should replace EMACTiva with EMACSnow |
| TIRTOS-158 | Watchdog examples should be re-designated to not reset the MCU |
| TIRTOS-164 | FAT SD example missing \n in print statement “Creating a new file …” (line 124 fatsd.c) |
| TIRTOS-176 | TI-RTOS examples single .cfg and use Mod_construct instead of Mod.create in the .cfg files |
| TIRTOS-184 | Need to move doxygen generation into drivers.git and out of zumaprod |
| TIRTOS-222 | Testlink tests generation should be separated by generation, building, and submissions. |
| TIRTOS-227 | Build warning for TI-RTOS |
| TIRTOS-228 | TI-RTOS should support IAR for MSP430 version 6.10 |
| TIRTOS-250 | Changed Concerto TCP and UDP examples to pass regression tests |
| TIRTOS-256 | UDP echo WiFi example only gets IP address every other program load |
| TIRTOS-263 | Legacy BIOS should be removed from all permutations of TI-RTOS |
| TIRTOS-309 | Top-level docs HTML’s doxygen link is wrong |
| TIRTOS-74 | Bigtime example does not build for MSP430F5529 |
| TIRTOS-78 | Move to IAR ARM 7.50.x in /db/vendors |
| TIRTOS-81 | Remove the example list table from the TI-RTOS GSGs (it gets stale quickly and not very useful) |
| TIRTOS-83 | TI-RTOS User’s guide needs instructions for setting project debugger options for MSP432 IAR |
| TIRTOS-86 | Merge the two TI-RTOS power management docs to one that covers: CC26xx/CC13xx, CC3200 and MSP432 |
| TIRTOS-87 | Remove bogus ‘exports’ directory at the top of the TI-RTOS installed directory |
| TIRTOS-99 | The drivers’ ROV documentation should be removed from the U.G. |
The following is a summary of known compatibility issues from previous releases:
This release requires the following other software components and tools.
Please check out the TI-RTOS Support Wiki for information about issues with this product.
All releases have 4 digits (M.mm.pp.bb). This includes GA and engineering releases. Engineering releases are denoted with an _eng suffix (e.g., 2.00.00.15_eng)
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory (e.g. tirtos_2_00_00_16).
Subsequent releases of patch upgrades will be identified by the patch number, ex. TI-RTOS 1.00.01.68 with directory tirtos_1_00_01_68. Typically, these patches only include critical bug fixes.