From RTSC-Pedia
![]() | [printable version] [offline version] | offline version generated on 27-May-2010 18:05 UTC | ![]() |
XDCspec - @InstanceInitError
This module's instance initialization can fail
This attribute is applicable only to modules with instances. If this attribute is specified for a module, its internal instance initialization function (Mod_Instance_init) is passed an Error_Block pointer (as its third parameter) so that it can raise an error. In addition, this function must always return a non-negative integer value. If an error is raised, the return value from this function is passed to any Mod_Instance_finalize method (in the second parameter)
If Mod_Instance_init returns -1, the finalize method is not passed a second parameter(!) and, depending on how the finalize method uses this parameter, may result in undefined program behavior(!).
The examples below illustrate the instance initialization method signature for a module named Foo both with and without the @InstanceInitError attribute.
| with @InstanceInitError | |
| | #include <xdc/runtime/Error.h>
#include "package/internal/Foo.xdc.h"
Int Foo_Instance_init(Foo_Object *obj, const Foo_Params *params, Error_Block *eb)
{
:
return (0);
} |
| without @InstanceInitError | |
| | #include "package/internal/Foo.xdc.h"
Void Foo_Instance_init(Foo_Object *obj, const Foo_Params *params)
{
:
} |
![]() | [printable version] [offline version] | offline version generated on 27-May-2010 18:05 UTC | ![]() |