Container for third party jars required by XDCtools
The following jars are part of this package:
[
more ... ]
| XDCspec declarations |
sourced in xdc/shelf/package.xdc |
package xdc.shelf [1, 0, 0] {
}
DETAILS
The following jars are part of this package:
In addition to the jars above, XDCtools requires the following
third-party command line executables:
Although the following tools are not required, they are optionally shipped
with XDCtools distributions to ensure consistent behavior across various
development platforms.
All other files that are part of XDCtools are licensed under either
EPL v1.0 or dual-licensed under
EDL v1.0.
generated on Sat, 01 Aug 2009 01:26:34 GMT