![]() |
![]() |
|
Framework Components Application Programming Interface (API)
fc-v02
|
This header defines all types and constants used in the XDAS interfaces.

Go to the source code of this file.
Macros | |
| #define | XDAS_TRUE 1 |
| #define | XDAS_FALSE 0 |
Typedefs | |
| typedef Void | XDAS_Void |
| typedef Uint8 | XDAS_Bool |
| typedef Int8 | XDAS_Int8 |
| typedef Uint8 | XDAS_UInt8 |
| typedef Int16 | XDAS_Int16 |
| typedef Uint16 | XDAS_UInt16 |
| typedef Int32 | XDAS_Int32 |
| typedef Uint32 | XDAS_UInt32 |