By default, the compiler program places the object and temporary files that it creates into the current directory. If you want the compiler program to place these files in different directories, use the following options:
| --asm_directory=directory | Specifies a directory for assembly files. For example:
cl7x --asm_directory=d:\assembly
|
| --obj_directory=directory | Specifies a directory for object files. For example:
cl7x --obj_directory=d:\object
|
| --output_file=filename | Specifies a compilation output file name; can override --obj_directory . For example:
cl7x --output_file=transfer
|
| --pp_directory=directory | Specifies a preprocessor file directory for object files (default is .). For example:
cl7x --pp_directory=d:\preproc
|
| --temp_directory=directory | Specifies a directory for temporary intermediate files. For example:
cl7x --temp_directory=d:\temp
|