Software pipelining schedules instructions from a loop so that multiple iterations of the loop execute in parallel. At optimization levels --opt_level=2 (or -O2) and --opt_level=3 (or -O3), the compiler usually attempts to software pipeline your loops. The --opt_for_speed option also affects the compiler's decision to attempt to software pipeline loops. In general, code size and performance are better when you use the --opt_level=2 or --opt_level=3 options. (See Section 4.1.)
Figure 4-1 illustrates a software-pipelined loop. The stages of the loop are represented by A, B, C, D, and E. In this figure, a maximum of five iterations of the loop can execute at one time. The shaded area represents the loop kernel. In the loop kernel, all five stages execute in parallel. The area above the kernel is known as the pipelined loop prolog, and the area below the kernel is known as the pipelined loop epilog.