12.8.4 Generating Copy Tables With the table() Operator
The linker supports extensions to the linker command file syntax that enable you to do the following:
- Identify any object components that may need to be copied from load space to run space at some point during the run of an application
- Instruct the linker to automatically generate a copy table that contains (at least) the load address, run address, and size of the component that needs to be copied
- Instruct the linker to generate a symbol specified by you that provides the address of a linker-generated copy table. For instance, Example 14 can be written as shown in Example 15: