5.13.5 Built-In Functions
The following built-in functions are supported:
- __builtin_abs()
- __builtin_constant_p()
- __builtin_expect()
- __builtin_fabs()
- __builtin_fabsf()
- __builtin_frame_address()
- __builtin_labs()
- __builtin_memcpy()
- __builtin_return_address()
The __builtin_frame_address() function always returns zero.
The __builtin_return_address() function always returns zero.