The compiler supports the 1989, 1999, and 2011 versions of the C language and the 2014 version of the C++ language. The C and C++ language features in the compiler are implemented in conformance with the following ISO standards:
The C compiler supports the 1989, 1999, and 2011 versions of the C language.
The compiler uses the C++14 version of the C++ standard. See the C++ Standard ISO/IEC 14882:2014. For a description of unsupported C++ features, see Section 5.2.
The compiler tools come with an extensive run-time library. Library functions conform to the ISO C/C++ library standard unless otherwise stated. The library includes functions for standard input and output, string manipulation, dynamic memory allocation, data conversion, timekeeping, trigonometry, and exponential and hyperbolic functions. Functions for signal handling are not included, because these are target-system specific. For more information, see Section 7.
See Section 5.12 for command line options to select the C or C++ standard your code uses.