The compiler allows interrupts to be disabled around software pipelined loops for threshold cycles within the function. This implements the --interrupt_threshold option for a single function (see Section 3.12). The FUNC_INTERRUPT_THRESHOLD pragma always overrides the --interrupt_threshold=n command line option. A threshold value less than 0 assumes that the function is never interrupted, which is equivalent to an interrupt threshold of infinity.
The syntax of the pragma in C is:
| #pragma FUNC_INTERRUPT_THRESHOLD (func,threshold) |
The syntax of the pragma in C++ is:
| #pragma FUNC_INTERRUPT_THRESHOLD (threshold) |
The following examples demonstrate the use of different thresholds:
#pragma FUNC_INTERRUPT_THRESHOLD (foo, 2000)
#pragma FUNC_INTERRUPT_THRESHOLD (foo, 1)
#pragma FUNC_INTERRUPT_THRESHOLD (foo, -1)