The CODE_SECTION pragma allocates space for the symbol in C, or the next symbol declared in C++, in a section named section name.
The syntax of the pragma in C is:
| #pragma CODE_SECTION (symbol, "section name") |
The syntax of the pragma in C++ is:
| #pragma CODE_SECTION ("section name") |
The CODE_SECTION pragma is useful if you have code objects that you want to link into an area separate from the .text section.
The following example demonstrates the use of the CODE_SECTION pragma.