The __x128_t Container Type

The __x128_t container type is available when compiling for C6600 only, It stores 128-bits of data and its use is necessary when performing certain SIMD operations on C6600. Also, note the leading double underscore. When using the __x128_t container type, you must include c6x.h.

This type can be used to define objects that can be used with certain C6600 intrinsics. (See Table 8-7.) The object can be filled and manipulated using various intrinsics. The type is not a full-fledged built-in type (like long long), and so various native C operations are not allowed. Think of this type as a struct with private members and special manipulation functions.

When the compiler puts a __x128_t object in the register file, the __x128_t object takes four registers (a register quad). Objects of type __x128_t are aligned to a 64-bit boundary in memory.

When an __x128_t object is passed on the stack, it is placed on a 64-bit boundary relative to the beginning of the stack. (The stack itself is aligned to a 64-bit boundary by default.) See the note in Section 8.6.2 for details.

The following operations are supported:

The following operations are not supported: