Register Conventions

Strict conventions associate specific registers with specific operations in the C/C++ environment. If you plan to interface an assembly language routine to a C/C++ program, you must understand and follow these register conventions.

The register conventions dictate how the compiler uses registers and how values are preserved across function calls. Table 8-2 summarizes how the compiler uses the TMS320C6000 registers.

The registers in Table 8-2 are available to the compiler for allocation to register variables and temporary expression results. If the compiler cannot allocate a register of a required type, spilling occurs. Spilling is the process of moving a register's contents to memory to free the register for another purpose.

Objects of type double, long, long long, or long double are allocated into an odd/even register pair and are always referenced as a register pair (for example, A1:A0). The odd register contains the sign bit, the exponent, and the most significant part of the mantissa. The even register contains the least significant part of the mantissa. The A4 register is used with A5 for passing the first argument if the first argument is a double, long, long long, or long double. The same is true for B4 and B5 for the second parameter, and so on. For more information about argument-passing registers and return registers, see Section 8.4.

Table 8-2 Register Usage

Register Function
Preserved By
Special Uses Register Function
Preserved By
Special Uses
A0 Parent – B0 Parent –
A1 Parent – B1 Parent –
A2 Parent – B2 Parent –
A3 Parent Structure register
(pointer to returned structure)(1)
B3 Parent Return register
(address to return to)
A4 Parent Argument 1 or return value B4 Parent Argument 2
A5 Parent Argument 1 or return value with A4 for doubles, longs and long longs B5 Parent Argument 2 with B4 for doubles, longs and long longs
A6 Parent Argument 3 B6 Parent Argument 4
A7 Parent Argument 3 with A6 for doubles, longs, and long longs B7 Parent Argument 4 with B6 for doubles, longs, and long longs
A8 Parent Argument 5 B8 Parent Argument 6
A9 Parent Argument 5 with A8 for doubles, longs, and long longs B9 Parent Argument 6 with B8 for doubles, longs, and long longs
A10 Child Argument 7 B10 Child Argument 8
A11 Child Argument 7 with A10 for doubles, longs, and long longs B11 Child Argument 8 with B10 for doubles, longs, and long longs
A12 Child Argument 9 B12 Child Argument 10
A13 Child Argument 9 with A12 for doubles, longs, and long longs B13 Child Argument 10 with B12 for doubles, longs, and long longs
A14 Child – B14 Child Data page pointer (DP)
A15 Child Frame pointer (FP) B15 Child Stack pointer (SP)
A16-A31 Parent B16-B31 Parent
ILC Child Loop buffer counter NRP Parent
IRP Parent RILC Child Loop buffer counter
Structs of size 64 or less are passed by value in registers instead of by reference using a pointer in A3.

All other control registers are not saved or restored by the compiler.

The compiler assumes that control registers not listed in Table 8-2 that can have an effect on compiled code have default values. For example, the compiler assumes all circular addressing-enabled registers are set for linear addressing (the AMR is used to enable circular addressing). Enabling circular addressing and then calling a C/C++ function without restoring the AMR to a default setting violates the calling convention. You must be certain that control registers which affect compiler-generated code have a default value when calling a C/C++ function from assembly.

Assembly language programmers must be aware that the linker assumes B15 contains the stack pointer. The linker needs to save and restore values on the stack in trampoline code that it generates. If you do not use B15 as the stack pointer in assembly code, you should use the linker option that disables trampolines, --trampolines=off. Otherwise, trampolines could corrupt memory and overwrite register values.