By default, the linker uses automatic library selection to select the correct run-time-support library (see Section 6.3.1.1) for your application. If you select the library manually, you must select the matching library according to the following naming scheme:
rtstrg[endian][abi][eh].lib
| trg | The device family of the C6000 architecture that the library was built for. This can be one of the following: 64plus, 6740, or 6600. | |
| endian | Indicates endianness: | |
| (blank) | Little-endian library | |
| e | Big-endian library | |
| abi | Indicates the application binary interface (ABI) used. Although the COFF file format is no longer supported, the library filename still contains "_elf" to distinguish the EABI libraries from older COFF libraries. | |
| _elf | EABI | |
| eh | Indicates whether the library has exception handling support | |
| (blank) | exception handling not supported | |
| _eh | exception handling support | |