L2: ; PIPED LOOP KERNEL
ADD .L2 B7,B4,B4 ; |14| <0,7> sum0 += a[0]*b[0]
|| ADD .L1 A5,A0,A0 ; |15| <0,7> sum1 += a[1]*b[1]
|| MPY .M2X B6,A4,B7 ; |12| <2,5> a[0] * b[0]
|| MPYH .M1X B6,A4,A5 ; |13| <2,5> a[1] * b[1]
|| [ B0] B .S1 L2 ; |18| <5,2> if (!I) goto loop
|| [ B0] ADD .S2 0xffffffff,B0,B0 ; |17| <6,1> I--
|| LDW .D2T2 *B5++,B6 ; |10| <7,0> load a[0-1] bank0
|| LDW .D1T1 *A3++,A4 ; |11| <7,0> load b[0-1] bank2
|| LDW *B0, B1
It is not always possible to control fully how arrays and other memory objects are aligned. This is especially true when a pointer is passed into a function and that pointer may have different alignments each time the function is called. A solution to this problem is to write a dot product routine that cannot have memory hits. This would eliminate the need for the arrays to use different memory banks.
If the dot product loop kernel is unrolled once, then four LDW instructions execute in the loop kernel. Assuming that nothing is known about the bank alignment of arrays a and b (except that they are word aligned), the only safe assumptions that can be made about the array accesses are that a[0-1] cannot conflict with a[2-3] and that b[0-1] cannot conflict with b[2-3]. Example 10 shows the unrolled loop kernel.