The C/C++ compiler provides diagnostic options to control compiler- and linker-generated diagnostic messages. The diagnostic options must be specified before the --run_linker option.
| --diag_error=num | Categorizes the diagnostic identified by num as an error. To determine the numeric identifier of a diagnostic message, use the --display_error_number option first in a separate compile. Then use --diag_error=num to recategorize the diagnostic as an error. You can only alter the severity of discretionary diagnostic messages. |
| --diag_remark=num | Categorizes the diagnostic identified by num as a remark. To determine the numeric identifier of a diagnostic message, use the --display_error_number option first in a separate compile. Then use --diag_remark=num to recategorize the diagnostic as a remark. You can only alter the severity of discretionary diagnostic messages. |
| --diag_suppress=num | Suppresses the diagnostic identified by num. To determine the numeric identifier of a diagnostic message, use the --display_error_number option first in a separate compile. Then use --diag_suppress=num to suppress the diagnostic. You can only suppress discretionary diagnostic messages. |
| --diag_warning=num | Categorizes the diagnostic identified by num as a warning. To determine the numeric identifier of a diagnostic message, use the --display_error_number option first in a separate compile. Then use --diag_warning=num to recategorize the diagnostic as a warning. You can only alter the severity of discretionary diagnostic messages. |
| --display_error_number | Displays a diagnostic's numeric identifier along with its text. Use this option in determining which arguments you need to supply to the diagnostic suppression options (--diag_suppress, --diag_error, --diag_remark, and --diag_warning). This option also indicates whether a diagnostic is discretionary. A discretionary diagnostic is one whose severity can be overridden. A discretionary diagnostic includes the suffix -D; otherwise, no suffix is present. See Section 3.7. |
| --emit_warnings_as_
errors |
Treats all warnings as errors. This option cannot be used with the --no_warnings option. The --diag_remark option takes precedence over this option. This option takes precedence over the --diag_warning option. |
| --issue_remarks | Issues remarks (non-serious warnings), which are suppressed by default. |
| --no_warnings | Suppresses diagnostic warnings (errors are still issued). |
| --section_sizes={on|off} | Generates section size information, including sizes for sections containing executable code and constants, constant or initialized data (global and static variables), and uninitialized data. Section size information is output during both the assembly and linking phases. This option should be placed on the command line with the compiler options (that is, before the --run_linker or --z option). |
| --set_error_limit=num | Sets the error limit to num, which can be any decimal value. The compiler abandons compiling after this number of errors. (The default is 100.) |
| --verbose_diagnostics | Provides verbose diagnostic messages that display the original source with line-wrap and indicate the position of the error in the source line. Note that this command-line option cannot be used within the Code Composer Studio IDE. |
| --write_diagnostics_file | Produces a diagnostic message information file with the same source file name with an .err extension. (The --write_diagnostics_file option is not supported by the linker.) Note that this command-line option cannot be used within the Code Composer Studio IDE. |