Make All Global Symbols Static (--make_static Option)

The --make_static option makes all global symbols static. Static symbols are not visible to externally linked modules. By making global symbols static, global symbols are essentially hidden. This allows external symbols with the same name (in different files) to be treated as unique.

The --make_static option effectively nullifies all .global assembler directives. All symbols become local to the module in which they are defined, so no external references are possible. For example, assume file1.obj and file2.obj both define global symbols called EXT. By using the --make_static option, you can link these files without conflict. The symbol EXT defined in file1.obj is treated separately from the symbol EXT defined in file2.obj.

cl6x --run_linker --make_static file1.obj file2.obj

The --make_static option makes all global symbols static. If you have a symbol that you want to remain global and you use the --make_static option, you can use the --make_global option to declare that symbol to be global. The --make_global option overrides the effect of the --make_static option for the symbol that you specify. The syntax for the --make_global option is:

--make_global=global_symbol