Example 16. Default Allocation for TMS320C6000 Devices

MEMORY { RAM : origin = 0x00000001, length = 0xFFFFFFFE } SECTIONS { .text : ALIGN(32) {} > RAM .const : ALIGN(8) {} > RAM .data : ALIGN(8) {} > RAM .bss : ALIGN(8) {} > RAM .cinit : ALIGN(4) {} > RAM ; cflag option only .pinit : ALIGN(4) {} > RAM ; cflag option only .stack : ALIGN(8) {} > RAM ; cflag option only .far : ALIGN(8) {} > RAM ; cflag option only .sysmem: ALIGN(8) {} > RAM ; cflag option only .switch: ALIGN(4) {} > RAM ; cflag option only .cio : ALIGN(4) {} > RAM ; cflag option only }

Also see Section 2.5.1 for information about default memory allocation.

All .text input sections are concatenated to form a .text output section in the executable output file, and all .data input sections are combined to form a .data output section.

If you use a SECTIONS directive, the linker performs no part of this default allocation. Instead, allocation is performed according to the rules specified by the SECTIONS directive and the general algorithm described next in Section 8.7.1.