The linker uses certain C/C++ compiler options to control linker-generated diagnostics. The diagnostic options must be specified before the --run_linker option.
| --diag_error=num | Categorize the diagnostic identified by num as an error. To find the numeric identifier of a diagnostic message, use the --display_error_number option first in a separate link. Then use --diag_error=num to recategorize the diagnostic as an error. You can only alter the severity of discretionary diagnostics. |
| --diag_remark=num | Categorize the diagnostic identified by num as a remark. To find the numeric identifier of a diagnostic message, use the --display_error_number option first in a separate link. Then use --diag_remark=num to recategorize the diagnostic as a remark. You can only alter the severity of discretionary diagnostics. |
| --diag_suppress=num | Suppress the diagnostic identified by num. To find the numeric identifier of a diagnostic message, use the --display_error_number option first in a separate link. Then use --diag_suppress=num to suppress the diagnostic. You can only suppress discretionary diagnostics. |
| --diag_warning=num | Categorize the diagnostic identified by num as a warning. To find the numeric identifier of a diagnostic message, use the --display_error_number option first in a separate link. Then use --diag_warning=num to recategorize the diagnostic as a warning. You can only alter the severity of discretionary diagnostics. |
| --display_error_number | Display a diagnostic's numeric identifier along with its text. Use this option in determining which arguments you need to supply to the diagnostic suppression options (--diag_suppress, --diag_error, --diag_remark, and --diag_warning). This option also indicates whether a diagnostic is discretionary. A discretionary diagnostic is one whose severity can be overridden. A discretionary diagnostic includes the suffix -D; otherwise, no suffix is present. See the TMS320C6000 Optimizing Compiler User's Guide for more information on understanding diagnostic messages. |
| --emit_warnings_as_
errors |
Treat all warnings as errors. This option cannot be used with the --no_warnings option. The --diag_remark option takes precedence over this option. This option takes precedence over the --diag_warning option. |
| --issue_remarks | Issue remarks (nonserious warnings), which are suppressed by default. |
| --no_warnings | Suppress warning diagnostics (errors are still issued). |
| --set_error_limit=num | Set the error limit to num, which can be any decimal value. The linker abandons linking after this number of errors. (The default is 100.) |
| --verbose_diagnostics | Provide verbose diagnostics that display the original source with line-wrap and indicate the position of the error in the source line |