6.14.1 C99 Support (--c99)
The compiler supports the 1999 standard of C as standardized by the ISO. However, the following list of run-time functions and features are not implemented or fully supported:
- complex.h
- ctype.h
- fenv.h
- float.h
- DECIMAL_DIG
- FLT_EVAL_METHOD
- inttypes.h
- wcstoimax() / wcstoumax()
- math.h: The math library used by the compiler in C99 mode has been changed. Full C99 math support is now available, including long double (64-bit) and float versions of floating point math routines. See the list of standard math.h C99 routines.
- stdarg.h
- stdio.h
- %a and %A format specifiers for hexadecimal float
- The %e specifier may produce "-0" when "0" is expected by the standard
- snprintf() does not properly pad with spaces when writing to a wide character array
- stdlib.h
- strtof() atof() / strtod() / strtold() do not support hexadecimal float strings
- vfscanf() / vscanf() / vsscanf() return value on floating point matching failure is incorrect
- tgmath.h
- time.h
- wchar.h
- getws() / fputws()
- mbrlen()
- mbsrtowcs()
- wcscat()
- wcschr()
- wcscmp() / wcsncmp()
- wcscpy() / wcsncpy()
- wcsftime()
- wcsrtombs()
- wcsstr()
- wcstok()
- wcsxfrm()
- Wide character print / scan functions
- Wide character conversion functions