Characteristics of TMS320C28x C++

The C28x compiler supports C++ as defined in the ANSI/ISO/IEC 14882:2003 standard (C++03), including these features:

The compiler supports the 2003 standard of C++ as standardized by the ISO. However, the following features are not implemented or fully supported: