C11 Support (--c11)

The compiler supports the 2011 standard of C as standardized by the ISO. However, in addition to the list in Section 6.15.1, the following run-time functions and features are not implemented or fully supported in C11 mode: