Special Section Types (DSECT, COPY, NOLOAD, and NOINIT)

You can assign the following special types to output sections: DSECT, COPY, NOLOAD, and NOINIT. The NOINIT type is supported for EABI only. These types affect the way that the program is treated when it is linked and loaded. You can assign a type to a section by placing the type after the section definition. For example:

SECTIONS { sec1: load = 0x00002000, type = DSECT {f1.obj} sec2: load = 0x00004000, type = COPY {f2.obj} sec3: load = 0x00006000, type = NOLOAD {f3.obj} sec4: load = 0x00008000, type = NOINIT {f4.obj} }