Example 18. Default Allocation for TMS320C28x Devices

MEMORY { PAGE 0: PROG: origin = 0x000040 length = 0x3fffc0 PAGE 1: DATA: origin = 0x000000 length = 0x010000 PAGE 1: DATA1: origin = 0x010000 length = 0x3f0000 } SECTIONS { .text: PAGE = 0 .data: PAGE = 0 .cinit: PAGE = 0 /* Used only for C programs */ .ebss: PAGE = 1 }

See Section 2.5.1 for information about default memory allocation.

All .text input sections are concatenated to form a .text output section in the executable output file, and all .data input sections are combined to form a .data output section.

If you use a SECTIONS directive, the linker performs no part of this default allocation. Instead, allocation is performed according to the rules specified by the SECTIONS directive and the general algorithm described next in Section 8.7.1.