/**************************************************/
/* Sample command file with SECTIONS directive */
/**************************************************/
file1.c.obj file2.c.obj /* Input files */
--output_file=prog.out /* Options */
SECTIONS
{
.text: load = PROG, PAGE = 0,
run = 0x0200, PAGE = 1
.econst: load = RAM1
.ebss: load = RAM1
.scratch: load = 0x0060, PAGE = 1
{
t1.c.obj(.scratch1)
t2.c.obj(.scratch2)
endscratch = .;
}
.data:alpha: align = 16
.data:beta: align = 16
}
Figure 8-3 shows the output sections defined by the SECTIONS directive in Example 5 (.vectors, .text, .econst, .ebss, .data:alpha, and .data:beta) and shows how these sections are allocated in memory using the MEMORY directive given in Example 3.