Example 1. Reference Implementation of a CRC Calculation Function: ref_crc.c

/*****************************************************************************/ /* Reference implementation of a CRC calculation function */ /* */ /* gen_crc is the interface function which should be called from the */ /* application. There is also a stand-alone test mode that can be used */ /* if _RUN_MAIN is defined. */ /*****************************************************************************/ /*---------------------------------------------------------------------------*/ /* This file does NOT implement a general-purpose CRC function. */ /* Specifically, it does not handle parameterization by initial value, bit */ /* reflection, or final XOR value. This implementation is intended only to */ /* implement the CRC functions used by the linker for C28x CRC tables. The */ /* algorithms used by the linker are selected to match the CRC algorithms in */ /* the PRIME and IEEE 802.15.4-2006 standards, which use the polynomials */ /* supported by the C28x VCU hardware. To understand CRCs in general, */ /* especially what other parameters exist, see: */ /* */ /* "A Painless Guide To CRC Error Detection Algorithms" likely at: */ /* http://www.ross.net/crc/download/crc_v3.txt */ /* Author : Ross Williams (ross@guest.adelaide.edu.au.). */ /* Date : 3 June 1993. */ /* Status : Public domain (C code). */ /*---------------------------------------------------------------------------*/ #include <stdio.h> #include <stdlib.h> #include <limits.h> /*---------------------------------------------------------------------------*/ /* These are the CRC algorithms supported by the linker, which match the */ /* polynomials supported in C28x VCU hardware, which match the PRIME and */ /* IEEE 802.15.4-2006 standards. These must match the values in crc_tbl.h. */ /*---------------------------------------------------------------------------*/ #define CRC32_PRIME 0 #define CRC16_802_15_4 1 #define CRC16_ALT 2 #define CRC8_PRIME 3 typedef struct crc_config_t { int id; int degree; unsigned long poly; } crc_config_t; const crc_config_t crc_config[] = { { CRC32_PRIME, 32, 0x04c11db7 }, { CRC16_802_15_4, 16, 0x1021 }, { CRC16_ALT, 16, 0x8005 }, { CRC8_PRIME, 8, 0x07 } }; unsigned long crc_table[256] = { 0 }; const crc_config_t *find_config(int id) { size_t i; for (i = 0; i < sizeof(crc_config) / sizeof(*crc_config); i++) if (crc_config[i].id == id) return &crc_config[i]; fprintf(stderr, "invalid config id %d\n", id); exit(EXIT_FAILURE); return NULL; } /*---------------------------------------------------------------------------*/ /* Table-driven version */ /*---------------------------------------------------------------------------*/ unsigned long generate_mask(int degree) { unsigned long half = (1ul << (degree / 2)) - 1; return half << (degree / 2) | half; } void generate_crc_table(const crc_config_t *config) { int i, j; unsigned long bit, crc; unsigned long high_bit = (1ul << (config->degree - 1)); unsigned long mask = generate_mask(config->degree); for (i = 0; i < 256; i++) { crc = (unsigned long)i << config->degree - 8; for (j = 0; j < 8; j++) { bit = crc & high_bit; crc <<= 1; if (bit) crc^= config->poly; } crc_table[i] = crc & mask; } } /*****************************************************************************/ /* gen_crc - Return the CRC value for the data using the given CRC algorithm */ /* int id : identifies the CRC algorithm */ /* char *data : the data */ /* size_t len : the size of the data */ /*****************************************************************************/ unsigned long gen_crc(int id, const unsigned char *data, size_t len) { /*-----------------------------------------------------------------------*/ /* Note: this is not a general-purpose CRC function. It does not handle */ /* parameterization by initial value, bit reflection, or final XOR */ /* value. This CRC function is specialized to the CRC algorithms in the */ /* linker used for C28x CRC tables. */ /*-----------------------------------------------------------------------*/ /*-----------------------------------------------------------------------*/ /* This CRC function is not intended to be optimal; it is written such */ /* that it works and generates the same result on all 8-bit and 16-bit */ /* targets, including C28x, other TI DSPs, and typical desktops. */ /*-----------------------------------------------------------------------*/ const crc_config_t *config = find_config(id); unsigned long crc = 0; unsigned long mask = generate_mask(config->degree); size_t i; generate_crc_table(config); for (i = 0; i < len; i++) { unsigned int datum = data[i]; /*--------------------------------------------------------------------*/ /* This loop handles 16-bit chars when we compile on 16-bit machines. */ /*--------------------------------------------------------------------*/ int n; for (n = 0; n < (CHAR_BIT / 8); n++) { /*----------------------------------------------------------------*/ /* For 16-bit machines, we need to feed the octets in an */ /* arbitrary order. For C2000, the arbitrary order we choose is */ /* to feed the LEAST significant octet of char 0 first. The */ /* first octet fed to the CRC is the LEAST-significant octet of */ /* char 0; the second octet is the MOST-significant octet of char */ /* 0. See the "Special Note regarding 16-bit char" in the */ /* Assembly Language Tools User's Guide. */ /*----------------------------------------------------------------*/ #if __TMS320C28XX__ /*----------------------------------------------------------------*/ /* Using __byte is not necessary; we use it here to illustrate */ /* how it relates to octet order. */ /*----------------------------------------------------------------*/ unsigned long octet = __byte((int*)&datum, n); #else unsigned long octet = ((datum >> (8 * n)) & 0xff); #endif unsigned long term1 = (crc << 8); int idx = ((crc >> (config->degree - 8)) & 0xff) ^ octet; crc = term1 ^ crc_table[idx]; } } return crc & mask; } #ifdef _RUN_MAIN /*****************************************************************************/ /* main - If requested, compute the CRC of test data using each algorithm. */ /*****************************************************************************/ int main(void) { #if CHAR_BIT == 16 const unsigned char data[] = { 'a', 'b', 'c', 'd' }; #elif CHAR_BIT == 8 /*-----------------------------------------------------------------------*/ /* This represents "abcd" as it would appear in C2000 memory if we view */ /* C2000 memory as octets, least-significant octet first; see "a special */ /* note regarding 16-bit char" in Assembly Language Tools User's Guide. */ /*-----------------------------------------------------------------------*/ const unsigned char data[] = { 'a', 0, 'b', 0, 'c', 0, 'd', 0 }; #endif /* CRC_8_PRIME: 0x70 */ /* CRC_16_802: 0x1bd3 */ /* CRC_32_PRIME: 0x4beab53b */ const unsigned char *p = (const unsigned char *)data; unsigned long crc; crc = gen_crc(CRC32_PRIME, p, sizeof data); printf("CRC_32_PRIME: %08lx\n", crc); crc = gen_crc(CRC8_PRIME, p, sizeof data); printf("CRC_8_PRIME: %02lx\n", crc); crc = gen_crc(CRC16_802_15_4, p, sizeof data); printf("CRC16_802_15_4: %04lx\n", crc); return 0; } #endif