8.8.5.5 Compression Algorithms
The following subsections provide information about decompression algorithms for the RLE and LZSS formats. To see example decompression algorithms, refer to the following functions in the Run-Time Support library:
- RLE: The __TI_decompress_rle() function in the copy_decompress_rle.c file.
- LZSS: The __TI_decompress_lzss() function in the copy_decompress_lzss.c file.
Additional information about compression algorithms can be found in the C28x Embedded Application Binary Interface Application Report (SPRAC71) EABI specification.
Run Length Encoding (RLE):
| 16-bit index |
Initialization data compressed using run length encoding |
The data following the 16-bit index is compressed using run length encoded (RLE) format. C2000 uses a simple run length encoding that can be decompressed using the following algorithm. See copy_decompress_rle.c for details.
- Read the first 16 bits, Delimiter (D).
- Read the next 16 bits (B).
- If B != D, copy B to the output buffer and go to step 2.
- Read the next 16 bits (L).
- If L == 0, then length is either a 32 bit value or we’ve reached the end of the data, read the next 16 bits (L).
- If L == 0, the end of the data is reached. Go to the "end of processing" step.
- If L !=0, then L is the most significant 16-bits of the 32-bit run length, L.hi. Read the next 16-bits, which is L.lo. Concatenate L.hi with L.lo to form the 32-bit run length.
- Else if L > 0 and L < 4, copy D to the output buffer L times. Go to step 2.
- Else, length is 16-bit value (L).
- Read the next 16 bits (C); C is the repeat character.
- Write C to the output buffer L times; go to step 2.
- End of processing.
The C2000 run-time support library has a routine __TI_decompress_rle() to decompress data compressed using RLE. The first argument to this function is the address pointing to the 16 bits after the 16-bit index. The second argument is the run address from the C auto initialization record.
Lempel-Ziv-Storer-Szymanski Compression (LZSS):
| 16-bit index |
Data compressed using LZSS |
The data following the 8-bit index is compressed using LZSS compression. The C2000 run-time-support library has the routine __TI_decompress_lzss() to decompress the data compressed using LZSS. The first argument to this function is the address pointing to the 16 bits after the 16-bit Index, and the second argument is the run address from the C auto initialization record.
The decompression algorithm for LZSS is as follows. See copy_decompress_lzss.c for details on the LZSS algorithm.
- Read 16 bits, which are the encoding flags (F) marking the start of the next LZSS encoded packet.
- For each bit (B) in F, starting from the least significant to the most significant bit, do the following:
- If (B & 0x1), read the next 16 bits and write it to the output buffer. Then advance to the next bit (B) in F and repeat this step.
- Else read the next 16-bits into temp (T), length (L) = (T & 0xf) + 2, and offset (O) = (T >> 4).
- If L == 17, read the next 16-bits (L'); then L += L'.
- If O == LZSS end of data (LZSS_EOD), we've reached the end of the data, and the algorithm is finished.
- At position (P) = output buffer - Offset (O) - 1, read L bytes from position P and write them to the output buffer.
- Go to step 2a.