The following GCC function attributes are supported:
The following additional TI-specific function attribute is supported:
For example, this function declaration uses the alias attribute to make "my_alias" a function alias for the "myFunc" function:
void my_alias() __attribute__((alias("myFunc")));
    The format attribute is applied to the declarations of printf, fprintf, sprintf, snprintf, vprintf, vfprintf, vsprintf, vsnprintf, scanf, fscanf, vfscanf, vscanf, vsscanf, and sscanf in stdio.h. Thus when GCC extensions are enabled, the data arguments of these functions are type checked against the format specifiers in the format string argument and warnings are issued when there is a mismatch. These warnings can be suppressed in the usual ways if they are not desired.
See Section 5.11.17 for more about using the interrupt function attribute.
The malloc attribute is applied to the declarations of malloc, calloc, realloc and memalign in stdlib.h.
The ramfunc attribute specifies that a function will be placed in and executed from RAM. The ramfunc attribute allows the compiler to optimize functions for RAM execution, as well as to automatically copy functions to RAM on flash-based devices. For example:
__attribute__((ramfunc))
void f(void) {
   ... 
}
    The --ramfunc=on option specifies that all functions compiled with this option are placed in and executed from RAM, even if this function attribute is not used.
Newer TI linker command files support the ramfunc attribute automatically by placing functions with this attribute in the .TI.ramfunc section. If you have a linker command file that does not include a section specification for the .TI.ramfunc section, you can modify the linker command file to place this section in RAM. See the Placing functions in RAM wiki page for more about the ramfunc attribute and option. See the ARM Assembly Language Tools User's Guide for details on section placement.
The target attribute causes the function to be compiled in either ARM (32-bit) or Thumb (16-bit) mode. The target attribute has the same effect as using the CODE_STATE pragma. The following examples use the target attribute.
__attribute__((target("arm"))) void foo(int arg1, int arg2)
__attribute__((target("thumb"))) void foo(int arg1, int arg2)
    Note that the "pcs" attribute described in the ACLE specification is not supported.
The retain attribute has the same effect as the RETAIN pragma (Section 5.11.26). That is, the section that contains the function will not be omitted from conditionally linked output even if it is not referenced elsewhere in the application.