The RESET_ULP pragma resets the specified ULP Advisor rules to the state they were before any CHECK_ULP pragmas (see Section 5.11.3) were processed. For instance, if a rule was enabled on the command line but disabled in the source, the RESET_ULP pragma resets it to enabled. This pragma accepts the same format as the --advice:power option, except for the "none" keyword.
The syntax of the pragma in C is:
| #pragma RESET_ULP (" {all|rulespec} ") |
The rulespec parameter is a comma-separated list of rule numbers. See Section 5.4 for details. See www.ti.com/ulpadvisor for a list of rules.