The CHECK_MISRA pragma enables/disables MISRA C:2004 rules at the source level. The compiler option --check_misra must be used to enable checking in order for this pragma to function at the source level.
The syntax of the pragma in C is:
| #pragma CHECK_MISRA (" {all|required|advisory|none|rulespec} ") |
The rulespec parameter is a comma-separated list of rule numbers. See Section 5.3 for details.
The RESET_MISRA pragma can be used to reset any CHECK_MISRA pragmas; see Section 5.11.25.