Example 2. Map File Output From Example 1 Showing Memory Ranges

----------------------------------------------------- 00004000..00005fff Page=0 Width=8 "EPROM1" ----------------------------------------------------- OUTPUT FILES: rom4000.b0 [b0..b7] rom4000.b1 [b8..b15] CONTENTS: 00004000..0000487f .text 00004880..00005b7f FILL = 00000000 00005b80..00005fff .data ----------------------------------------------------- 00006000..00007fff Page=0 Width=8 "EPROM2" ----------------------------------------------------- OUTPUT FILES: rom6000.b0 [b0..b7] rom6000.b1 [b8..b15] CONTENTS: 00006000..0000633f .data 00006340..000066ff FILL = ff00ff00 00006700..00007c7f .table 00007c80..00007fff FILL = ff00ff00

EPROM1 defines the address range from 0x00004000 through 0x00005FFF with the following sections:

This section ... Has this range ...
.text 0x00004000 through 0x0000487F
.data 0x00005B80 through 0x00005FFF

The rest of the range is filled with 0h (the default fill value), converted into two output files:

EPROM2 defines the address range from 0x00006000 through 0x00007FFF with the following sections:

This section ... Has this range ...
.data 0x00006000 through 0x0000633F
.table 0x00006700 through 0x00007C7F

The rest of the range is filled with 0xFF00FF00 (from the specified fill value). The data from this range is converted into two output files: