Scenario 3 shows how to build the hex conversion command file for converting a object file for the memory system shown in Figure B-5. In this system, there are two external 64K × 16-bit EPROMs interfacing with the TMS470 target processor. The application code and data will be burned on the EPROM starting at address 0x20. The application code will be burned first, followed by the data tables.
In this scenario, the EPROM load address for the application code and for the data also corresponds to the TMS470 CPU address that accesses the code and data. Therefore, only a load address needs to be specified.
Example 7 shows the linker command file for this scenario.