Name Mangling

Symbol names may be mangled in C++ source files. When mangling occurs, the converted assembly will use the mangled names to avoid symbol name clashes. You can use the demangler (armdem) to demangle names and identify the correct symbols to use in assembly.

To defeat name mangling in C++ for symbols where polymorphism (calling a function of the same name with different kinds of arguments) is not required, use the following syntax:

extern "C" void somefunc(int arg);

The above format is the short method for declaring a single function. To use this method for multiple functions, you can also use the following syntax:

extern "C" { void somefunc(int arg); int anotherfunc(int arg); ... }