| armstrip |
is the command that invokes the strip utility. |
| input filename |
is an object file (.obj) or an executable file (.out). |
| options |
identifies the strip utility options you want to use. Options are not case sensitive and can appear anywhere on the command line following the invocation. Precede each option with a hyphen (-). The strip utility option is as follows: |
|
--help (-h) |
displays help information. |
|
--outfile (-o)filename |
writes the stripped output to filename. |
|
--postlink (-p) |
removes all information not required for execution. This option causes more information to be removed than the default behavior, but the object file is left in a state that cannot be linked. This option should be used only with executable (.out) files. |
|
--rom |
Strip readonly sections and segments. |
| When the strip utility is invoked without the -o option, the input object files are replaced with the stripped version. |