The FUNC_IS_PURE pragma specifies to the compiler that the named function has no side effects. This allows the compiler to do the following:
The pragma must appear before any declaration or reference to the function. In C, the argument func is the name of a function. In C++, the pragma applies to the next function declared.
The syntax of the pragma in C is:
| #pragma FUNC_IS_PURE (func) |
The syntax of the pragma in C++ is:
| #pragma FUNC_IS_PURE |