Performing File-Level Optimization (--opt_level=3 option)

The --opt_level=3 option (aliased as the -O3 option) instructs the compiler to perform file-level optimization. You can use the --opt_level=3 option alone to perform general file-level optimization, or you can combine it with other options to perform more specific optimizations. The options listed in Table 3-1 work with --opt_level=3 to perform the indicated optimization:

Table 3-1 Options That You Can Use With --opt_level=3

If You ... Use this Option See
Want to create an optimization information file --gen_opt_level=n Section 3.3.1
Want to compile multiple source files --program_level_compile Section 3.4